Header file for FrameQ on SharedMemory interface. (Deprecated)
#include <ti/ipc/GateMP.h>
Go to the source code of this file.
Data Structures | |
struct | FrameQ_ShMem_Params_tag |
Structure defining instance create parameters for the FrameQ on shared memory(inter core and intra core). More... | |
struct | FrameQ_ShMem_OpenParams_tag |
Structure defining open parameters for the FrameQ instance on ShMem (shared memory interface). More... | |
Typedefs | |
typedef FrameQ_Config | FrameQ_ShMem_Config |
typedef struct FrameQ_ShMem_Params_tag | FrameQ_ShMem_Params |
Structure defining instance create parameters for the FrameQ on shared memory(inter core and intra core). | |
typedef struct FrameQ_ShMem_OpenParams_tag | FrameQ_ShMem_OpenParams |
Structure defining open parameters for the FrameQ instance on ShMem (shared memory interface). | |
Functions | |
void | FrameQ_ShMem_Params_init (FrameQ_ShMem_Params *params) |
Function to initiallze the params with the default params. | |
UInt32 | FrameQ_ShMem_sharedMemReq (const FrameQ_ShMem_Params *params) |
Function to find out the shared memory requirements. | |
Void | FrameQ_ShMem_getConfig (FrameQ_ShMem_Config *cfg) |
Int32 | FrameQ_ShMem_setup (FrameQ_ShMem_Config *cfg) |
Int32 | FrameQ_ShMem_destroy (void) |
typedef FrameQ_Config FrameQ_ShMem_Config |
typedef struct FrameQ_ShMem_Params_tag FrameQ_ShMem_Params |
Structure defining instance create parameters for the FrameQ on shared memory(inter core and intra core).
typedef struct FrameQ_ShMem_OpenParams_tag FrameQ_ShMem_OpenParams |
Structure defining open parameters for the FrameQ instance on ShMem (shared memory interface).
void FrameQ_ShMem_Params_init | ( | FrameQ_ShMem_Params * | params ) |
Function to initiallze the params with the default params.
params | pointer to FrameQ_ShMem_Params. |
UInt32 FrameQ_ShMem_sharedMemReq | ( | const FrameQ_ShMem_Params * | params ) |
Function to find out the shared memory requirements.
This function returns size of the shared memory required for the instance based on the params provided.
params | pointer to FrameQ_ShMem_Params. |
size | shared memory reqired for the instance |
Void FrameQ_ShMem_getConfig | ( | FrameQ_ShMem_Config * | cfg ) |
Int32 FrameQ_ShMem_setup | ( | FrameQ_ShMem_Config * | cfg ) |
Int32 FrameQ_ShMem_destroy | ( | void | ) |