Data Fields

RingIO_Params_Tag Struct Reference

Common parameters required to create RingIO instance of any implementation. It should be the first element of the actual implementaton params structure . More...

#include <RingIO.h>

Data Fields

String name
RingIO_Type interfaceType

Detailed Description

Common parameters required to create RingIO instance of any implementation. It should be the first element of the actual implementaton params structure .


Field Documentation

Name of the instance

interface type for ringio delegate


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated