![]() |
![]() |
_Memory.h [code] | Memory manager interface definitions |
_MemoryDefs.h [code] | Definitions for Memory module |
_MemoryOS.h [code] | Memory abstraction APIs for local memory allocation |
Cache.h [code] | Defines Cache API interface |
Cfg.h [code] | Configuration Helper Utilities |
FrameQ.h [code] | Defines for interfaces for FrameQ module |
FrameQ_ShMem.h [code] | Header file for FrameQ on SharedMemory interface |
FrameQBufMgr.h [code] | Defines for interfaces for FrameQBufMgr module |
FrameQBufMgr_ShMem.h [code] | Header file for FrameQBufMgr ShMem |
FrameQBufMgrDefs.h [code] | Defines configurable elements for FrameQBufMgr module |
FrameQDefs.h [code] | Defines configurable elements for FrameQ module |
Gate.h [code] | Critical section support |
GateMonitor.h [code] | Header file for Gate based on Monitor |
GateMP.h [code] | Multiple processor gate that provides local and remote context protection |
GateMutex.h [code] | Gate based on Mutex |
GateProcess.h [code] | Process level gate |
GateSem.h [code] | Header file for Gate based on Semaphore |
GateSpinlock.h [code] | Gate based on Spinlock |
HeapBufMP.h [code] | Multi-processor fixed-size buffer heap implementation |
HeapMemMP.h [code] | Multi-processor variable size buffer heap implementation |
HeapMultiBufMP.h [code] | Multiple fixed size buffer heap implementation |
HeapQueueMgr.h [code] | Multi-processor fixed-size buffer heap using hardware queues |
IGateProvider.h [code] | Interface implemented by all gate providers |
IHeap.h [code] | Defines Heap based memory allocator |
Ipc.h [code] | Ipc Manager |
IpcHost.h [code] | This file contains APIs and defines that are used by applications only on the host-side of the device |
IpcMemMgr.h [code] | IPC Memory Manager |
List.h [code] | Creates a doubly linked list. It works as utils for other modules |
ListMP.h [code] | Multiple processor shared memory list |
Memory.h [code] | Memory manager interface definitions |
MemoryDefs.h [code] | Definitions for Memory module |
MemoryOS.h [code] | Memory abstraction APIs for local memory allocation |
MessageQ.h [code] | MessageQ Manager |
MultiProc.h [code] | Processor ID Manager |
NameServer.h [code] | NameServer Manager |
Notify.h [code] | Notification manager for IPC |
OsalPrint.h [code] | Kernel utils Print interface definitions |
OsalSemaphore.h [code] | Kernel utils Semaphore interface definitions |
ProcMgr.h [code] | The Processor Manager on a master processor provides control functionality for a slave device |
RingIO.h [code] | This will have definitions for interfaces and structures for RingIO module |
RingIOShm.h [code] | RingIOShm shared memory based physical transport for communication with the remote processor |
SharedRegion.h [code] | Shared memory manager and address translator |
Std.h [code] | This will have definitions of standard data types for platform abstraction |
String.h [code] | Defines for String manipulation library |
SysLink.h [code] | This module contains common definitions, types, structures and functions used by SysLink |
SyslinkMemMgr.h [code] | Header file implementing Memory manager. It is a wrapper implementation to support Shared memory allocation using heap address translations using shared region or Tiler buffer allocation using tiler buffer manager and address translations |
Trace.h [code] | Kernel Trace enabling/disabling/application interface |