Data Fields

RingIO_Config_Tag Struct Reference

Structure defining config parameters for the RingIO module. More...

#include <RingIO.h>

Data Fields

UInt32 maxNameLen
UInt32 maxInstances

Detailed Description

Structure defining config parameters for the RingIO module.


Field Documentation

Maximum length of the name of RingIO instance

Maximum number of RingIO's that can be made


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated