Data Fields

FrameQ_CreateParams_Tag Struct Reference

Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure . More...

#include <FrameQ.h>

Data Fields

UInt32 size
FrameQ_Interface ctrlInterfaceType
String name
Bool openFlag

Detailed Description

Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure .


Field Documentation

Size of the paramstructure

Interface type

Name of the instance


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated