Data Fields

FrameQBufMgr_Params Struct Reference

Common parameters required to create FrameQBufMgr instance of any implementation. More...

#include <FrameQBufMgr.h>

Collaboration diagram for FrameQBufMgr_Params:
Collaboration graph
[legend]

Data Fields

FrameQBufMgr_CreateParams commonCreateParams
Ptr impParams
UInt32 impParamsSize

Detailed Description

Common parameters required to create FrameQBufMgr instance of any implementation.

This struct must be the first element of the implementation-specific create params structure.


Field Documentation

Pointer to implementation-specific struct

Size of the implementation-specific impParams struct.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated