Data Fields

FrameQBufMgr_CreateParams_Tag Struct Reference

Common parameters required to create FrameQBufMgr instance of any implementation. More...

#include <FrameQBufMgr.h>

Data Fields

UInt32 size
FrameQBufMgr_Interface ctrlInterfaceType
String name
UInt32 openFlag

Detailed Description

Common parameters required to create FrameQBufMgr instance of any implementation.

This struct must be the first field of the implementation-specific params structure.


Field Documentation

size of param struct

Interface type

Instance name

Open flag to indicate create or open.

Remarks:
This is an internal flag, the caller should not touch this flag during create

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated