Data Fields

FrameQBufMgr_Params Struct Reference

Common parameters required to create FrameQBufMgr instance of any implementation. It should be the first element of the actual implementaton params structure . More...

#include <FrameQBufMgr.h>

Collaboration diagram for FrameQBufMgr_Params:
Collaboration graph
[legend]

Data Fields

FrameQBufMgr_CreateParams commonCreateParams
Ptr impParams
UInt32 impParamsSize

Detailed Description

Common parameters required to create FrameQBufMgr instance of any implementation. It should be the first element of the actual implementaton params structure .


Field Documentation

Pointer to implementation specific parameters

Size of the implementation specific structure pointed by impParams.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated