| typedef ITimer.IPeripheralArray |
 |
| typedef ITimer.StringArray |
 |
typedef String StringArray[];
| struct ITimer.ForceSetDefaultRegister_t |
 |
Force Set Default Register
metaonly struct ForceSetDefaultRegister_t {
String register;
Bool regForceSet;
};
DETAILS
Type to store if each register needs to be forced initialized
even if the register is in default state.
SEE
| struct ITimer.regIntVect_t |
 |
Interrupt vector description
metaonly struct regIntVect_t {
String registerName;
String registerDescription;
String isrToggleString;
String priorityName;
Bool interruptEnable;
Bool interruptHandler;
Int priority;
};
DETAILS
Type to describe a single interrupt vector pin and all its possible
configurations.
SEE
| ITimer.getAll() // module-wide |
 |
Find all peripherals of a certain type
DETAILS
The type of the peripherals returned is defined by the type of the
caller.
RETURNS
Returns an array of IPeripheral instances
| ITimer.getRegisters() // module-wide |
 |
Find all registers defined by the peripheral
RETURNS
Returns an array of register names
| config ITimer.baseAddr // instance |
 |
Address of the peripheral's control register
DETAILS
A peripheral's registers are commonly accessed through a structure
that defines the offsets of a particular register from the lowest
address mapped to a peripheral. That lowest address is specified by
this parameter.
| config ITimer.intNum // instance |
 |
Interrupt source number
| config ITimer.name // instance |
 |
Specific peripheral name given by the device
DETAILS
Devices can have more than one peripheral of the same type. In such
cases, device data sheets give different names to the instances of a
same peripheral. For example, the name for a timer module could be
TimerA3, and a device that has two such timers can name them TA0
and TA1.
| config ITimer.numberOfTimers // instance |
 |
Stores the number of available timer capture compare blocks
config UChar numberOfTimers;
| config ITimer.owner // instance |
 |
String specifying the entity that manages the peripheral
| Instance Creation |
 |
// Create an instance-object
| ITimer.getTxxCCRx() // instance |
 |
Returns TxxCCRx register value based on which CCR register
Bits16 getTxxCCRx(UChar ccrNumber);
SEE
| ITimer.setTxxCCRx() // instance |
 |
Sets TxxCCRx register value based on which CCR register
Void setTxxCCRx(UChar ccrNumber, Bits16 value);
SEE