This command allows RTSC content, in the form of reusable modules built
using the XDCtools tooling, to be imported into a system integrator's
embedded application. It is the recommended method for integrating RTSC
content into non-RTSC application build environments.
Configuro lets the system integrator identify and customize the RTSC
content they wish to use, and computes a set of libraries, command-line
flags and other artifacts to include in their application build. By
changing the values of configuration settings, the integrator can
trade off the functionality, memory footprint, and even performance of
the RTSC content to best meet the needs of their application.
config Main.usage // module-wide |
|
usage help message
XDCscript usage |
meta-domain |
Main.usage = String[] [
'[-v | -q]',
'[-@ optionsfile]',
'[-o outdir]',
'[-b config_bld | -c codegen_dir | --cb]',
'[-t target] [-p platform[:instance]] [-r profile]',
'[-Dname=value]',
'[-w | -x regexp]',
'[--rtsName pkg_name]',
'[--cfgArgs args_string]',
'[--linkTemplate linker_template]',
'[--tcf] [--bios5] [--pkg] [--generationOnly]',
'[--compileOptions compile_options_string]',
'[--oc compiler.opt] [--ol linker.cmd]',
'infile.cfg'
];
Main.exec() // module-wide |
|
'xs' script entry point
XDCscript usage |
meta-domain |
Main.exec(Any args) returns Any
Main.main() // module-wide |
|
'xs' shell entry point
XDCscript usage |
meta-domain |
Main.main(Any args) returns Any
Instance Config Parameters |
|
XDCscript usage |
meta-domain |
var params = new Main.Params;
// Instance config-params object
params.bios5Incs = Bool false;
// Add the DSP/BIOS 5.X include directory to the compiler options
params.cfgArgs = String null;
// Optional arguments passed to configuration script
params.compileOptions = String "";
// Add compile options for C files in the configuration package
params.compilerOptionsFile = String "compiler.opt";
// Set the name of the compiler options file (default is "compiler.opt")
params.configbld = String null;
// Read build environment from the named config.bld file
params.defines = String[] [ ];
// Set a Java property in the configuration script
params.exclude = String null;
// Exclude packages matching regexp from compatibility checking
params.generationOnly = Bool false;
// Create the configuration generated source files but do not build
params.hasTconf = Bool false;
// Read infile.tcf in addition to infile.cfg
params.linkTemplate = String null;
// Linker command file template
params.linkerCommandFile = String "linker.cmd";
// Set the name of the linker command file (default is "linker.cmd")
params.mkPkgOnly = Bool false;
// Create the build model generated output files but do not build
params.output = String null;
// Pathname of the output directory
params.platform = String null;
// Name of the RTSC platform package (and optionally instance)
params.profile = String 'release';
// Build profile to use
params.quiet = Bool false;
// Minimize details during build
params.rootdir = String null;
// Root directory of the code generation tools
params.rtsName = String null;
// Set the name of the RTSC runtime package
params.searchForConfigBld = Bool false;
// Use a config.bld found along the package path
params.target = String null;
// Name of the RTSC target module
params.verbose = Bool false;
// Show verbose details during build
params.warn = Bool false;
// Treat package version incompatibilites as warnings
config Main.bios5Incs // instance |
|
Add the DSP/BIOS 5.X include directory to the compiler options
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.bios5Incs = Bool false;
DETAILS
The directory is located in "include" in package "ti.bios".
config Main.cfgArgs // instance |
|
Optional arguments passed to configuration script
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.cfgArgs = String null;
DETAILS
Lets the user pass values into the configuration script from the
command line. The argument is an expression in JavaScript syntax.
Its value is available in the configuration script under the name
Program.build.cfgArgs.
The JavaScript expression is evaluated in the configuration domain
after the platform package is imported, immediately before calling
the user's configuration script.
This string has the same effect as the
cfgArgs string in
xdc.bld.Executable.Attrs.
You can pass multiple values to configuration scripts using the
syntax of a JavaScript Object constant:
xs xdc.tools.configuro --cfgArgs "{foo:'hello';bar:2}" ... app.cfg
The configuration script can read the various fields as, e.g.:
if (Program.build.cfgArgs.foo == "hello") {
:
}
Note the use of single quotes around the string value 'hello' on
the command line. This is the easiest way to quote a JavaScript
string constant that is compatible with the enclosing double
quotes, which are for the benefit of the command line shell.
SEE
config Main.compileOptions // instance |
|
Add compile options for C files in the configuration package
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.compileOptions = String "";
DETAILS
This option accepts one or more compiler options that are added to
the compiler command line when compiling C files in the generated
configuration package.
If multiple compiler options are given, the whole string containing
options must be surrounded by quotes.
config Main.compilerOptionsFile // instance |
|
Set the name of the compiler options file (default is "compiler.opt")
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.compilerOptionsFile = String "compiler.opt";
config Main.configbld // instance |
|
Read build environment from the named config.bld file
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.configbld = String null;
DETAILS
A config.bld file can optionally be used to hold the values
of the target, compiler root directory, platform, and other
more advanced options. This is a convenient way to share a common
build environment between multiple projects.
The format of the file is JavaScript statements with the XDCscript
extensions. The script should set the properties of the
Build global object.
If no config.bld file is given then the target and compiler
root directory are required command-line parameters.
config Main.defines // instance |
|
Set a Java property in the configuration script
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.defines = String[] [ ];
DETAILS
Allows values to be injected from the command line into the
config.bld file. For example, the option -Dmyprop=myval
creates a property named myprop with string value "myval".
This can be read in config.bld using the XDCscript syntax
environment["myprop"].
config Main.exclude // instance |
|
Exclude packages matching regexp from compatibility checking
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.exclude = String null;
DETAILS
A JavaScript regular expression that is used to select packages that
should be excluded from the set of packages checked during
configuration.
SEE
config Main.generationOnly // instance |
|
Create the configuration generated source files but do not build
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.generationOnly = Bool false;
DETAILS
This option runs the configuration step but does not compile the
generated source files. This option is used
by internal tooling to eliminate unnecessary build steps.
config Main.hasTconf // instance |
|
Read infile.tcf in addition to infile.cfg
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.hasTconf = Bool false;
DETAILS
The .tcf file optionally configures DSP/BIOS 5.X . This allows a
single program to use both DSP/BIOS 5.X and RTSC-based content.
config Main.linkTemplate // instance |
|
Linker command file template
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.linkTemplate = String null;
DETAILS
If this option is provided it overrides the template supplied by
the platform, giving the caller complete control over the generated
linker command file.
SEE
config Main.linkerCommandFile // instance |
|
Set the name of the linker command file (default is "linker.cmd")
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.linkerCommandFile = String "linker.cmd";
config Main.mkPkgOnly // instance |
|
Create the build model generated output files but do not build
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.mkPkgOnly = Bool false;
DETAILS
This option creates the output directory and key generated files
but does not process the user's configuration script. It is used
by internal tooling to snapshot the RTSC build settings implied by
the configuro command line parameters.
config Main.output // instance |
|
Pathname of the output directory
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.output = String null;
DETAILS
A directory containing the generated build artifacts, in particular
the compiler.opt and linker.cmd files. By default, the output
directory has the same name as the configuration script, minus the
.cfg extension, within the same parent directory as this script.
config Main.platform // instance |
|
Name of the RTSC platform package (and optionally instance)
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.platform = String null;
DETAILS
The name of a RTSC platform package to use, using the syntax
my.pkg.name or my.pkg.name:instanceName. For example,
ti.platforms.sim64Pxx or ti.platforms.generic:custom.
This is an optional parameter, and by default the platform is
the one that the selected target names as its default. The user
may override this default in their config.bld or by using this
parameter.
The optional
:instanceName suffix names a pre-configured variant
of the platform, which can be set up either in the user's
config.bld or in the platform package itself. For more details, see
Build.platformTable
and the
IPlatform interface.
config Main.profile // instance |
|
Build profile to use
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.profile = String 'release';
DETAILS
The name of the build profile to use for the RTSC content, for
example 'release' or 'debug'. The list of allowed profiles is
determined by the RTSC target module named.
config Main.quiet // instance |
|
Minimize details during build
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.quiet = Bool false;
DETAILS
This option produces the same output as the xdc command
with the XDCOPTIONS=qq parameter.
config Main.rootdir // instance |
|
Root directory of the code generation tools
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.rootdir = String null;
DETAILS
The path to the installation directory of the compiler and linker
for the selected target. The definition of "installation directory"
can vary from compiler to compiler, but is most commonly the
directory that contains a "bin" subdirectory.
If no config.bld file is given, then this is a required
parameter.
If a config.bld file is given then this parameter is optional,
and by default the compiler will be the one configured there.
This option can still be used, to override the default established
in config.bld.
config Main.rtsName // instance |
|
Set the name of the RTSC runtime package
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.rtsName = String null;
DETAILS
The name of a package containing pre-built libraries containing
the
xdc.runtime modules. If this parameter is
null (or
undefined) the name of the rts package is taken from the target
(
xdc.bld.ITarget.rtsName). If this parameter is set to
the empty string (""), then no rts package is included in the
configuration. Finally, if this parameter is non-
null and
non-empty, it should be the name of a package along the package
path that can supply pre-built versions of the modules in the
xdc.runtime package.
SEE
config Main.searchForConfigBld // instance |
|
Use a config.bld found along the package path
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.searchForConfigBld = Bool false;
DETAILS
Find a config.bld by searching the package path, instead of
via an explicit pathname. Looks for a file named config.bld in
any of the directories named along the package path, in order. The
directories are not searched recursively.
config Main.target // instance |
|
Name of the RTSC target module
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.target = String null;
DETAILS
The name of a RTSC target module to use, for example
ti.targets.C64P.
If no config.bld file is given, then this is a required
parameter.
If a
config.bld file is given then this parameter is optional,
and by default the target will be
Build.targets[0] from the
user's
config.bld. If
Build.targets contains more than one entry,
then this option can be used to override that default.
config Main.verbose // instance |
|
Show verbose details during build
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.verbose = Bool false;
DETAILS
This option produces the same verbose output as the xdc command
with the XDCOPTIONS=v parameter.
config Main.warn // instance |
|
Treat package version incompatibilites as warnings
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.warn = Bool false;
DETAILS
If set to "true", force any incompatibilities detected to be
treated as warnings only; otherwise incompatibilities are fatal.
SEE
Main.gen() // instance |
|
Generate and build the configuration package
XDCscript usage |
meta-domain |
inst.gen(String infile) returns Int
Main.run() // instance |
|
Underlying implementation
XDCscript usage |
meta-domain |