package xdc.tools.configuro |
![]() |
Command-line configuration tool
XDCspec declarations | sourced in xdc/tools/configuro/package.xdc |
A directory containing the generated build artifacts, in particular the compiler.opt and linker.cmd files. By default, the output directory has the same name as the configuration script, minus the .cfg extension, within the same parent directory as this script.
The name of a RTSC target module to use, for example ti.targets.C64P.
If no config.bld file is given, then this is a required parameter.
If a config.bld file is given then this parameter is optional, and by default the target will be Build.targets[0] from the user's config.bld. If Build.targets contains more than one entry, then this option can be used to override that default.
The path to the installation directory of the compiler and linker for the selected target. The definition of "installation directory" can vary from compiler to compiler, but is most commonly the directory that contains a "bin" subdirectory.
If no config.bld file is given, then this is a required parameter.
If a config.bld file is given then this parameter is optional, and by default the compiler will be the one configured there. This option can still be used, to override the default established in config.bld.
The name of a RTSC platform package to use, using the syntax my.pkg.name or my.pkg.name:instanceName. For example, ti.platforms.sim64Pxx or ti.platforms.generic:custom.
This is an optional parameter, and by default the platform is the one that the selected target names as its default. The user may override this default in their config.bld or by using this parameter.
The optional :instanceName suffix names a pre-configured variant of the platform, which can be set up either in the user's config.bld or in the platform package itself. For more details, see Build.platformTable and the IPlatform interface.
The name of the build profile to use for the RTSC content, for example 'release' or 'debug'. The list of allowed profiles is determined by the RTSC target module named.
A config.bld file can optionally be used to hold the values of the target, compiler root directory, platform, and other more advanced options. This is a convenient way to share a common build environment between multiple projects.
The format of the file is JavaScript statements with the XDCscript extensions. The script should set the properties of the Build global object.
If no config.bld file is given then the target and compiler root directory are required command-line parameters.
Find a config.bld by searching the package path, instead of via an explicit pathname. Looks for a file named config.bld in any of the directories named along the package path, in order. The directories are not searched recursively.
Allows values to be injected from the command line into the config.bld file. For example, the option -Dmyprop=myval creates a property named myprop with string value "myval". This can be read in config.bld using the XDCscript syntax environment["myprop"].
The name of a package containing pre-built libraries containing the xdc.runtime modules. If this parameter is null (or undefined) the name of the rts package is taken from the target (xdc.bld.ITarget.rtsName). If this parameter is set to the empty string (""), then no rts package is included in the configuration. Finally, if this parameter is non-null and non-empty, it should be the name of a package along the package path that can supply pre-built versions of the modules in the xdc.runtime package.
Lets the user pass values into the configuration script from the command line. The argument is an expression in JavaScript syntax. Its value is available in the configuration script under the name Program.build.cfgArgs.
The JavaScript expression is evaluated in the configuration domain after the platform package is imported, immediately before calling the user's configuration script.
This string has the same effect as the cfgArgs string in xdc.bld.Executable.Attrs.
You can pass multiple values to configuration scripts using the syntax of a JavaScript Object constant:
xs xdc.tools.configuro --cfgArgs "{foo:'hello';bar:2}" ... app.cfg
The configuration script can read the various fields as, e.g.:
if (Program.build.cfgArgs.foo == "hello") { : }
Note the use of single quotes around the string value 'hello' on the command line. This is the easiest way to quote a JavaScript string constant that is compatible with the enclosing double quotes, which are for the benefit of the command line shell.
If this option is provided it overrides the template supplied by the platform, giving the caller complete control over the generated linker command file.
This option produces the same verbose output as the xdc command with the XDCOPTIONS=v parameter.
This option produces the same output as the xdc command with the XDCOPTIONS=qq parameter.
A JavaScript regular expression that is used to select packages that should be excluded from the set of packages checked during configuration.
If set to "true", force any incompatibilities detected to be treated as warnings only; otherwise incompatibilities are fatal.
The .tcf file optionally configures DSP/BIOS 5.X . This allows a single program to use both DSP/BIOS 5.X and RTSC-based content.
The directory is located in "include" in package "ti.bios".
This option creates the output directory and key generated files but does not process the user's configuration script. It is used by internal tooling to snapshot the RTSC build settings implied by the configuro command line parameters.
This option runs the configuration step but does not compile the generated source files. This option is used by internal tooling to eliminate unnecessary build steps.
This option accepts one or more compiler options that are added to the compiler command line when compiling C files in the generated configuration package. If multiple compiler options are given, the whole string containing options must be surrounded by quotes.
xs xdc.tools.configuro myconfig.cfg