SemThread Manager. [EXPERIMENTAL]
This module manages semaphores through its proxy ISemThreadSupport
interface. It has a module wide config parameter
Proxy which needs to be bound to an OS specific delegate before
this module can be used.
Here is an example showing how the proxy is bound to an BIOS 6.x specific
delegate.
var SemThread = xdc.useModule('xdc.runtime.knl.SemThread');
SemThread.Proxy = xdc.useModule('ti.sysbios.xdcruntime.SemThreadSupport');
Typically the package containing the delegates have a Settings module that
will bind all
xdc.runtime.knl proxies. The following
example sets up all the xdc.runtime.knl proxies.
proxy SemThread.Proxy |
![](../../../Arrow_up.png) |
Proxy that needs to be bound to an OS specific delegate
XDCscript usage |
meta-domain |
// explicit access to the currently bound delegate module
SemThread.Proxy.abstractInstances$ = false
// use indirect runtime function calls if true
const SemThread.FOREVER |
![](../../../Arrow_up.png) |
Used as the timeout value to specify wait forever
XDCscript usage |
meta-domain |
const SemThread.FOREVER = ~(0);
#define SemThread_FOREVER (UInt)~(0)
enum SemThread.Mode |
![](../../../Arrow_up.png) |
Types of semaphores
XDCscript usage |
meta-domain |
values of type SemThread.Mode
const SemThread.Mode_COUNTING;
// Counting semaphore
const SemThread.Mode_BINARY;
// Binary Semaphore
typedef enum SemThread_Mode {
SemThread_Mode_COUNTING,
// Counting semaphore
SemThread_Mode_BINARY
// Binary Semaphore
} SemThread_Mode;
enum SemThread.PendStatus |
![](../../../Arrow_up.png) |
Error codes returned by Semaphore_pend
XDCscript usage |
meta-domain |
values of type SemThread.PendStatus
const SemThread.PendStatus_ERROR;
const SemThread.PendStatus_TIMEOUT;
const SemThread.PendStatus_SUCCESS;
typedef enum SemThread_PendStatus {
SemThread_PendStatus_ERROR,
SemThread_PendStatus_TIMEOUT,
SemThread_PendStatus_SUCCESS
} SemThread_PendStatus;
metaonly config SemThread.common$ // module-wide |
![](../../../Arrow_up.png) |
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
module-wide built-ins |
![](../../../Arrow_up.png) |
// Get this module's unique id
Bool SemThread_Module_startupDone( );
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool SemThread_Module_hasMask( );
// Test whether this module has a diagnostics mask
Bits16 SemThread_Module_getMask( );
// Returns the diagnostics mask for this module
Void SemThread_Module_setMask( Bits16 mask );
// Set the diagnostics mask for this module
per-instance object types |
![](../../../Arrow_up.png) |
typedef struct SemThread_Object SemThread_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct SemThread_Struct SemThread_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
per-instance config parameters |
![](../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new SemThread.Params;
// Instance config-params object
// Semaphore mode. Default is COUNTING
typedef struct SemThread_Params {
// Instance config-params structure
// Common per-instance configs
// Semaphore mode. Default is COUNTING
} SemThread_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config SemThread.mode // per-instance |
![](../../../Arrow_up.png) |
Semaphore mode. Default is COUNTING
XDCscript usage |
meta-domain |
var params = new SemThread.Params;
...
DETAILS
When mode is BINARY , the semaphore has only two states, available
and unavailable. When mode is COUNTING, the semaphore keeps track of
number of times a semaphore is posted.
per-instance creation |
![](../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params =
new SemThread.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = SemThread.create( Int count, params );
// Create an instance-object
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
count
initial semaphore count
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
This function creates a new SemThread object which is initialized to
count.
per-instance deletion |
![](../../../Arrow_up.png) |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
SemThread.pend( ) // per-instance |
![](../../../Arrow_up.png) |
Wait for the semaphore to become available
ARGUMENTS
handle
handle of a previously-created SemThread instance object
timeout
timeout in microseconds
eb
error block
DETAILS
RETURNS
refer to description above
SemThread.post( ) // per-instance |
![](../../../Arrow_up.png) |
Increment the semaphore count
ARGUMENTS
handle
handle of a previously-created SemThread instance object
eb
error block
RETURNS
true for success, false for error in error block
per-instance convertors |
![](../../../Arrow_up.png) |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
per-instance built-ins |
![](../../../Arrow_up.png) |
Int SemThread_Object_count( );
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object