metaonly module xdc.tools.path.sg.Main |
![](../../../../Arrow_up.png) |
Graphical interface to path tool
This graphical interactive tool displays the packages located along any
specified package repository path.
[
more ... ]
metaonly module Main { ...
XDCscript usage |
meta-domain |
var Main = xdc.useModule('xdc.tools.path.sg.Main');
module-wide functions
metaonly module Main {
module-wide functions
}
USAGE
DETAILS
This graphical interactive tool displays the packages located along any
specified package repository path.
At startup, this tool shows the packages located along the current package
path; i.e.,
$XDCPATH;$XDCROOT/packages;^
where $XDCPATH is the value of the the user settable prefix of the
package path, $XDCROOT is the installation directory of the XDC tools,
and ^ is the repository of the package in the current working directory
(if it exists).
BUGS
This tool scans all packages available along the current
package path before displaying the user interface. So, a repository in
the package path that contains a large number of sub-directories, such
as '/', causes very long delays before the user interface is displayed.
While it is easy to see that you should not put '/' in the package path,
it is less obvious that installing a package at '/' has the same effect.
Main.main( ) // module-wide |
![](../../../../Arrow_up.png) |
Main entry point for interactive interface to path tool
XDCscript usage |
meta-domain |
Main.main( Any args ) returns Any
generated on Thu, 25 Jun 2009 21:45:59 GMT