1 /*
2 *Copyright (c) 2008 Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12 /*!
13 * ======== Main ========
14 * Graphical interface to path tool
15 *
16 * This graphical interactive tool displays the packages located along any
17 * specified package repository path.
18 *
19 * At startup, this tool shows the packages located along the current package
20 * path; i.e.,
21 * @p(code) 22 * $XDCPATH;$XDCROOT/packages;^
23 * @p 24 *
25 * where `$XDCPATH` is the value of the the user settable prefix of the
26 * package path, `$XDCROOT` is the installation directory of the XDC tools,
27 * and `^` is the repository of the package in the current working directory
28 * (if it exists).
29 *
30 * @b(Usage) 31 * @p(code) 32 * xs xdc.tools.path.sg
33 * @p 34 *
35 * @a(Bugs) 36 *
37 * This tool scans all packages available along the current
38 * package path before displaying the user interface. So, a repository in
39 * the package path that contains a large number of sub-directories, such
40 * as '/', causes very long delays before the user interface is displayed.
41 *
42 * While it is easy to see that you should not put '/' in the package path,
43 * it is less obvious that installing a package at '/' has the same effect.
44 */
45 metaonlymodule Main
46 {
47
48 /*!
49 * ======== main ========
50 * Main entry point for interactive interface to path tool
51 */
52 function main(args);
53
54 /*!
55 * ======== createPartControl ========
56 * @_nodoc 57 */
58 function createPartControl(parent, viewPart);
59 }
60 /*
61 * @(#) xdc.tools.path.sg; 1, 0, 0,130; 6-9-2009 14:23:21; /db/ztree/library/trees/xdctools-c16x/src/
62 */
63