![]() |
![]() |
Functions | |
int | Sock6PrAttach (SOCK6 *ps) |
int | Sock6PrDetach (SOCK6 *ps) |
void | Sock6PrCtlError (SOCK6 *ps, uint Code) |
int Sock6PrAttach | ( | SOCK6 * | ps | ) |
Description
The function attaches the SOCKET to the appropriate global family list.
[in] | ps | The pointer to the socket which we will attach to the corresponding list. |
Success | - 0 | |
Error | - Non Zero |
void Sock6PrCtlError | ( | SOCK6 * | ps, | |
uint | Code | |||
) |
Description
The function notifies the socket of a problem. Sets the appropriate error code on the socket.
[in] | ps | The pointer to the socket to which the error needs to be notified. |
[in] | Code | Error code indicating the problem. |
None |
int Sock6PrDetach | ( | SOCK6 * | ps | ) |
Description
The function detaches the SOCKET from the appropriate global family list.
[in] | ps | The pointer to the socket which we will detach from the corresponding list. |
Success | - 0 | |
Error | - Non Zero |