![]() |
![]() |
#include <sockif.h>
Collaboration diagram for SOCK6:
Data Fields | |
FILEDESC | fd |
File descriptor header. | |
UINT8 | Family |
Address family of the socket (AF_INET6). | |
UINT8 | SockType |
Socket Type (SOCK_STREAM/SOCK_DGRAM/SOCK_RAW). | |
UINT8 | Protocol |
IP Protocol (TCP/UDP/ICMPV6 etc). | |
UINT32 | FlowLabel |
Flow label associated with the socket. | |
UINT8 | HopLimit |
Hop Limit for Unicast packets. | |
UINT32 | ScopeId |
Scope ID associated with the socket. | |
UINT16 | SockPriority |
Socket Priority. | |
UINT32 | SockProt |
Socket Protocol Handler (SOCKPROT_NONE/SOCKPROT_TCP/ SOCKPROT_UDP/SOCKPROT_RAW). | |
uint | OptionFlags |
Socket Option flags (SO_...) as defined in socket.h. | |
uint | StateFlags |
Socket State flags (SS_...). Defined and used by NDK core stack internally. | |
UINT32 | dwLingerTime |
Time used when SO_LINGER set. | |
SOCK6 * | pProtNext |
Pointer to next socket in protocol list. | |
SOCK6 * | pProtPrev |
Pointer to previous socket in protocol list. | |
IP6N | FIP |
Foreign Host's IPv6 Address. | |
UINT16 | FPort |
Foreign Host's Port. | |
IP6N | LIP |
Local IPv6 Address (NULL for wildcard). | |
UINT16 | LPort |
Local Port to which socket is bound (NULL if not bound). | |
IP6N | BIP |
IPv6 Address to which this socket is bound (valid for DGRAM sockets). | |
UINT16 | BPort |
Port to which this socket is bound (valid for DGRAM sockets). | |
HANDLE | hTP |
Handle to Protocol specific data. | |
HANDLE | hRoute6 |
Handle to the cached V6 Route. | |
HANDLE | hIFTx |
Handle to default Interface for transmit. | |
SOCK6 * | pParent |
Handle to the parent socket. | |
SOCK6 * | pPrevQ |
Previous Socket in Pending/ready queue. | |
SOCK6 * | pPending |
Pending connection sockets list. | |
SOCK6 * | pReady |
Ready/connected sockets list. | |
UINT32 | ConnMax |
Maximum allowed pending/ready connections on this socket. | |
UINT32 | ConnTotal |
Total number of current connections on socket. | |
int | ErrorPending |
Error returned on socket call. | |
INT32 | OOBMark |
Out of band info mark. | |
uint | OOBData |
Out of band info data. | |
UINT32 | RxTimeout |
Receive Timeout for stream sockets. | |
UINT32 | TxTimeout |
Transmit Timeout for stream sockets. | |
UINT32 | RxBufSize |
Receive buffer size. | |
UINT32 | TxBufSize |
Transmit buffer size. | |
HANDLE | hSBRx |
Handle to Receive buffer of the socket. | |
HANDLE | hSBTx |
Handle to Transmit buffer of the socket. |
This data structure identifies a socket used for communication over IPv6.