CC13xx Driver Library
ssi.c
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: ssi.c
3 * Revised: 2015-11-16 19:41:47 +0100 (Mon, 16 Nov 2015)
4 * Revision: 45094
5 *
6 * Description: Driver for Synchronous Serial Interface
7 *
8 * Copyright (c) 2015 - 2016, Texas Instruments Incorporated
9 * All rights reserved.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions are met:
13 *
14 * 1) Redistributions of source code must retain the above copyright notice,
15 * this list of conditions and the following disclaimer.
16 *
17 * 2) Redistributions in binary form must reproduce the above copyright notice,
18 * this list of conditions and the following disclaimer in the documentation
19 * and/or other materials provided with the distribution.
20 *
21 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
22 * be used to endorse or promote products derived from this software without
23 * specific prior written permission.
24 *
25 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
26 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
27 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
28 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
29 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
30 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
31 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
32 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
33 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
34 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
35 * POSSIBILITY OF SUCH DAMAGE.
36 *
37 ******************************************************************************/
38 
39 #include <driverlib/ssi.h>
40 
41 //*****************************************************************************
42 //
43 // Handle support for DriverLib in ROM:
44 // This section will undo prototype renaming made in the header file
45 //
46 //*****************************************************************************
47 #if !defined(DOXYGEN)
48  #undef SSIConfigSetExpClk
49  #define SSIConfigSetExpClk NOROM_SSIConfigSetExpClk
50  #undef SSIDataPut
51  #define SSIDataPut NOROM_SSIDataPut
52  #undef SSIDataPutNonBlocking
53  #define SSIDataPutNonBlocking NOROM_SSIDataPutNonBlocking
54  #undef SSIDataGet
55  #define SSIDataGet NOROM_SSIDataGet
56  #undef SSIDataGetNonBlocking
57  #define SSIDataGetNonBlocking NOROM_SSIDataGetNonBlocking
58  #undef SSIIntRegister
59  #define SSIIntRegister NOROM_SSIIntRegister
60  #undef SSIIntUnregister
61  #define SSIIntUnregister NOROM_SSIIntUnregister
62 #endif
63 
64 //*****************************************************************************
65 //
67 //
68 //*****************************************************************************
69 void
70 SSIConfigSetExpClk(uint32_t ui32Base, uint32_t ui32SSIClk,
71  uint32_t ui32Protocol, uint32_t ui32Mode,
72  uint32_t ui32BitRate, uint32_t ui32DataWidth)
73 {
74  uint32_t ui32MaxBitRate;
75  uint32_t ui32RegVal;
76  uint32_t ui32PreDiv;
77  uint32_t ui32SCR;
78  uint32_t ui32SPH_SPO;
79 
80  //
81  // Check the arguments.
82  //
83  ASSERT(SSIBaseValid(ui32Base));
84  ASSERT((ui32Protocol == SSI_FRF_MOTO_MODE_0) ||
85  (ui32Protocol == SSI_FRF_MOTO_MODE_1) ||
86  (ui32Protocol == SSI_FRF_MOTO_MODE_2) ||
87  (ui32Protocol == SSI_FRF_MOTO_MODE_3) ||
88  (ui32Protocol == SSI_FRF_TI) ||
89  (ui32Protocol == SSI_FRF_NMW));
90  ASSERT((ui32Mode == SSI_MODE_MASTER) ||
91  (ui32Mode == SSI_MODE_SLAVE) ||
92  (ui32Mode == SSI_MODE_SLAVE_OD));
93  ASSERT(((ui32Mode == SSI_MODE_MASTER) && (ui32BitRate <= (ui32SSIClk / 2))) ||
94  ((ui32Mode != SSI_MODE_MASTER) && (ui32BitRate <= (ui32SSIClk / 12))));
95  ASSERT((ui32SSIClk / ui32BitRate) <= (254 * 256));
96  ASSERT((ui32DataWidth >= 4) && (ui32DataWidth <= 16));
97 
98  //
99  // Set the mode.
100  //
101  ui32RegVal = (ui32Mode == SSI_MODE_SLAVE_OD) ? SSI_CR1_SOD : 0;
102  ui32RegVal |= (ui32Mode == SSI_MODE_MASTER) ? 0 : SSI_CR1_MS;
103  HWREG(ui32Base + SSI_O_CR1) = ui32RegVal;
104 
105  //
106  // Set the clock predivider.
107  //
108  ui32MaxBitRate = ui32SSIClk / ui32BitRate;
109  ui32PreDiv = 0;
110  do
111  {
112  ui32PreDiv += 2;
113  ui32SCR = (ui32MaxBitRate / ui32PreDiv) - 1;
114  }
115  while(ui32SCR > 255);
116  HWREG(ui32Base + SSI_O_CPSR) = ui32PreDiv;
117 
118  //
119  // Set protocol and clock rate.
120  //
121  ui32SPH_SPO = (ui32Protocol & 3) << 6;
122  ui32Protocol &= SSI_CR0_FRF_M;
123  ui32RegVal = (ui32SCR << 8) | ui32SPH_SPO | ui32Protocol | (ui32DataWidth - 1);
124  HWREG(ui32Base + SSI_O_CR0) = ui32RegVal;
125 }
126 
127 //*****************************************************************************
128 //
130 //
131 //*****************************************************************************
132 int32_t
133 SSIDataPutNonBlocking(uint32_t ui32Base, uint32_t ui32Data)
134 {
135  //
136  // Check the arguments.
137  //
138  ASSERT(SSIBaseValid(ui32Base));
139  ASSERT((ui32Data & (0xfffffffe << (HWREG(ui32Base + SSI_O_CR0) &
140  SSI_CR0_DSS_M))) == 0);
141 
142  //
143  // Check for space to write.
144  //
145  if(HWREG(ui32Base + SSI_O_SR) & SSI_SR_TNF)
146  {
147  HWREG(ui32Base + SSI_O_DR) = ui32Data;
148  return(1);
149  }
150  else
151  {
152  return(0);
153  }
154 }
155 
156 
157 //*****************************************************************************
158 //
160 //
161 //*****************************************************************************
162 void
163 SSIDataPut(uint32_t ui32Base, uint32_t ui32Data)
164 {
165  //
166  // Check the arguments.
167  //
168  ASSERT(SSIBaseValid(ui32Base));
169  ASSERT((ui32Data & (0xfffffffe << (HWREG(ui32Base + SSI_O_CR0) &
170  SSI_CR0_DSS_M))) == 0);
171 
172  //
173  // Wait until there is space.
174  //
175  while(!(HWREG(ui32Base + SSI_O_SR) & SSI_SR_TNF))
176  {
177  }
178 
179  //
180  // Write the data to the SSI.
181  //
182  HWREG(ui32Base + SSI_O_DR) = ui32Data;
183 }
184 
185 //*****************************************************************************
186 //
188 //
189 //*****************************************************************************
190 void
191 SSIDataGet(uint32_t ui32Base, uint32_t *pui32Data)
192 {
193  //
194  // Check the arguments.
195  //
196  ASSERT(SSIBaseValid(ui32Base));
197 
198  //
199  // Wait until there is data to be read.
200  //
201  while(!(HWREG(ui32Base + SSI_O_SR) & SSI_SR_RNE))
202  {
203  }
204 
205  //
206  // Read data from SSI.
207  //
208  *pui32Data = HWREG(ui32Base + SSI_O_DR);
209 }
210 
211 //*****************************************************************************
212 //
231 //
232 //*****************************************************************************
233 int32_t
234 SSIDataGetNonBlocking(uint32_t ui32Base, uint32_t *pui32Data)
235 {
236  //
237  // Check the arguments.
238  //
239  ASSERT(SSIBaseValid(ui32Base));
240 
241  //
242  // Check for data to read.
243  //
244  if(HWREG(ui32Base + SSI_O_SR) & SSI_SR_RNE)
245  {
246  *pui32Data = HWREG(ui32Base + SSI_O_DR);
247  return(1);
248  }
249  else
250  {
251  return(0);
252  }
253 }
254 
255 //*****************************************************************************
256 //
273 //
274 //*****************************************************************************
275 void
276 SSIIntRegister(uint32_t ui32Base, void (*pfnHandler)(void))
277 {
278  uint32_t ui32Int;
279 
280  //
281  // Check the arguments.
282  //
283  ASSERT(SSIBaseValid(ui32Base));
284 
285  //
286  // Determine the interrupt number based on the SSI port.
287  //
288  ui32Int = (ui32Base == SSI0_BASE) ? INT_SSI0_COMB : INT_SSI1_COMB;
289 
290  //
291  // Register the interrupt handler.
292  //
293  IntRegister(ui32Int, pfnHandler);
294 
295  //
296  // Enable the synchronous serial port interrupt.
297  //
298  IntEnable(ui32Int);
299 }
300 
301 //*****************************************************************************
302 //
315 //
316 //*****************************************************************************
317 void
318 SSIIntUnregister(uint32_t ui32Base)
319 {
320  uint32_t ui32Int;
321 
322  //
323  // Check the arguments.
324  //
325  ASSERT(SSIBaseValid(ui32Base));
326 
327  //
328  // Determine the interrupt number based on the SSI port.
329  //
330  ui32Int = (ui32Base == SSI0_BASE) ? INT_SSI0_COMB : INT_SSI1_COMB;
331 
332  //
333  // Disable the interrupt.
334  //
335  IntDisable(ui32Int);
336 
337  //
338  // Unregister the interrupt handler.
339  //
340  IntUnregister(ui32Int);
341 }
#define SSI_MODE_SLAVE_OD
Definition: ssi.h:130
void SSIDataGet(uint32_t ui32Base, uint32_t *pui32Data)
Gets a data element from the SSI receive FIFO.
Definition: ssi.c:191
#define SSI_FRF_MOTO_MODE_0
Definition: ssi.h:121
#define SSI_FRF_MOTO_MODE_2
Definition: ssi.h:123
int32_t SSIDataPutNonBlocking(uint32_t ui32Base, uint32_t ui32Data)
Puts a data element into the SSI transmit FIFO.
Definition: ssi.c:133
#define SSI_FRF_TI
Definition: ssi.h:125
#define ASSERT(expr)
Definition: debug.h:74
int32_t SSIDataGetNonBlocking(uint32_t ui32Base, uint32_t *pui32Data)
Gets a data element from the SSI receive FIFO.
Definition: ssi.c:234
void SSIDataPut(uint32_t ui32Base, uint32_t ui32Data)
Puts a data element into the SSI transmit FIFO.
Definition: ssi.c:163
#define SSI_MODE_SLAVE
Definition: ssi.h:129
void SSIIntRegister(uint32_t ui32Base, void(*pfnHandler)(void))
Registers an interrupt handler for the synchronous serial port.
Definition: ssi.c:276
void IntUnregister(uint32_t ui32Interrupt)
Unregisters the function to be called when an interrupt occurs.
Definition: interrupt.c:200
#define SSI_FRF_NMW
Definition: ssi.h:126
#define SSI_FRF_MOTO_MODE_3
Definition: ssi.h:124
void SSIIntUnregister(uint32_t ui32Base)
Unregisters an interrupt handler for the synchronous serial port.
Definition: ssi.c:318
#define SSI_FRF_MOTO_MODE_1
Definition: ssi.h:122
void SSIConfigSetExpClk(uint32_t ui32Base, uint32_t ui32SSIClk, uint32_t ui32Protocol, uint32_t ui32Mode, uint32_t ui32BitRate, uint32_t ui32DataWidth)
Configures the synchronous serial port.
Definition: ssi.c:70
#define SSI_MODE_MASTER
Definition: ssi.h:128
void IntDisable(uint32_t ui32Interrupt)
Disables an interrupt.
Definition: interrupt.c:378
void IntRegister(uint32_t ui32Interrupt, void(*pfnHandler)(void))
Registers a function to be called when an interrupt occurs.
Definition: interrupt.c:152
void IntEnable(uint32_t ui32Interrupt)
Enables an interrupt.
Definition: interrupt.c:318