CC13xx Driver Library
osc.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include <inc/hw_aon_wuc.h>
#include <inc/hw_types.h>
#include <inc/hw_memmap.h>
#include <inc/hw_ddi.h>
#include <inc/hw_ddi_0_osc.h>
#include <driverlib/rom.h>
#include <driverlib/ddi.h>
#include <driverlib/debug.h>

Go to the source code of this file.

Macros

#define LOW_POWER_XOSC   1
 
#define HIGH_POWER_XOSC   0
 
#define OSC_SRC_CLK_HF   0x00000001
 
#define OSC_SRC_CLK_MF   0x00000002
 
#define OSC_SRC_CLK_LF   0x00000004
 
#define OSC_RCOSC_HF   0x00000000
 
#define OSC_XOSC_HF   0x00000001
 
#define OSC_RCOSC_LF   0x00000002
 
#define OSC_XOSC_LF   0x00000003
 
#define SCLK_HF_RCOSC_HF   0
 
#define SCLK_HF_XOSC_HF   1
 
#define SCLK_MF_RCOSC_HF   0
 
#define SCLK_MF_XOSC_HF   1
 
#define SCLK_LF_FROM_RCOSC_HF   0
 
#define SCLK_LF_FROM_XOSC_HF   1
 
#define SCLK_LF_FROM_RCOSC_LF   2
 
#define SCLK_LF_FROM_XOSC_LF   3
 

Functions

static void OSCXHfPowerModeSet (uint32_t ui32Mode)
 Set Power Mode for High Frequency XTAL Oscillator. More...
 
static void OSCClockLossEventEnable (void)
 Enables OSC clock loss event detection. More...
 
static void OSCClockLossEventDisable (void)
 Disables OSC clock loss event detection. More...
 
void OSCClockSourceSet (uint32_t ui32SrcClk, uint32_t ui32Osc)
 Configure the oscillator input to the a source clock. More...
 
uint32_t OSCClockSourceGet (uint32_t ui32SrcClk)
 Get the source clock settings. More...
 
static bool OSCHfSourceReady (void)
 Check if the HF clock source is ready to be switched. More...
 
static void OSCHfSourceSwitch (void)
 Switch the high frequency clock. More...
 
static void OSCInterfaceEnable (void)
 Deprecated: Empty function - original functionality is removed. More...
 
static void OSCInterfaceDisable (void)
 Deprecated: Empty function - original functionality is removed. More...
 
uint32_t OSCHF_GetStartupTime (uint32_t timeUntilWakeupInMs)
 Returns maximum startup time (in microseconds) of XOSC_HF. More...
 
void OSCHF_TurnOnXosc (void)
 Turns on XOSC_HF (but without switching to XOSC_HF). More...
 
bool OSCHF_AttemptToSwitchToXosc (void)
 Switch to XOSC_HF if XOSC_HF is ready. More...
 
void OSCHF_SwitchToRcOscTurnOffXosc (void)
 Switch to RCOSC_HF and turn off XOSC_HF. More...
 
uint32_t OSCHF_DebugGetCrystalAmplitude (void)
 Get crystal amplitude (assuming crystal is running). More...
 
uint32_t OSCHF_DebugGetExpectedAverageCrystalAmplitude (void)
 Get the expected average crystal amplitude. More...
 
int32_t OSC_HPOSCRelativeFrequencyOffsetGet (int32_t tempDegC)
 Calculate the temperature dependent relative frequency offset of HPOSC. More...
 
int16_t OSC_HPOSCRelativeFrequencyOffsetToRFCoreFormatConvert (int32_t HPOSC_RelFreqOffset)
 Converts the relative frequency offset of HPOSC to the RF Core parameter format. More...