![]() |
![]() |
TI-RTOS for TivaC
2.14.04.31
|
USBMSCHFatFs driver implementation for a Tiva USB controller used with the USBMSCHFatFs driver.
============================================================================
The USBMSCHFatFs header file should be included in an application as follows:
This USBMSCHFatFs driver implementation is designed to operate with a Tiva' USB library. Only 1 instance of the USBMSCHFatFsTiva driver is supported.
#include <stdint.h>
#include <ti/drivers/USBMSCHFatFs.h>
#include <ti/sysbios/gates/GateMutex.h>
#include <ti/sysbios/family/arm/m3/Hwi.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <ti/sysbios/fatfs/ff.h>
#include <ti/sysbios/fatfs/diskio.h>
Go to the source code of this file.
Data Structures | |
struct | USBMSCHFatFsTiva_HWAttrs |
USBMSCHFatFsTiva Hardware attributes. More... | |
struct | USBMSCHFatFsTiva_Object |
USBMSCHFatFsTiva Object. More... | |
Macros | |
#define | ti_sysbios_family_arm_m3_Hwi__nolocalnames |
#define | HCDMEMORYPOOLSIZE 128 |
Typedefs | |
typedef unsigned long | USBMSCType |
typedef enum USBMSCHFatFsTiva_USBState | USBMSCHFatFsTiva_USBState |
USBMSCHFatFsTiva_USBState. More... | |
typedef struct USBMSCHFatFsTiva_HWAttrs | USBMSCHFatFsTiva_HWAttrs |
USBMSCHFatFsTiva Hardware attributes. More... | |
typedef struct USBMSCHFatFsTiva_Object | USBMSCHFatFsTiva_Object |
USBMSCHFatFsTiva Object. More... | |
typedef struct USBMSCHFatFsTiva_Object * | USBMSCHFatFsTiva_Handle |
Enumerations | |
enum | USBMSCHFatFsTiva_USBState { USBMSCHFatFsTiva_NO_DEVICE, USBMSCHFatFsTiva_CONNECTED, USBMSCHFatFsTiva_UNKNOWN, USBMSCHFatFsTiva_POWER_FAULT } |
USBMSCHFatFsTiva_USBState. More... | |
Variables | |
const USBMSCHFatFs_FxnTable | USBMSCHFatFsTiva_fxnTable |
#define ti_sysbios_family_arm_m3_Hwi__nolocalnames |
#define HCDMEMORYPOOLSIZE 128 |
typedef unsigned long USBMSCType |
typedef enum USBMSCHFatFsTiva_USBState USBMSCHFatFsTiva_USBState |
USBMSCHFatFsTiva_USBState.
typedef struct USBMSCHFatFsTiva_HWAttrs USBMSCHFatFsTiva_HWAttrs |
USBMSCHFatFsTiva Hardware attributes.
typedef struct USBMSCHFatFsTiva_Object USBMSCHFatFsTiva_Object |
USBMSCHFatFsTiva Object.
The application must not access any member variables of this structure!
typedef struct USBMSCHFatFsTiva_Object * USBMSCHFatFsTiva_Handle |
const USBMSCHFatFs_FxnTable USBMSCHFatFsTiva_fxnTable |