![]() |
![]() |
TI-RTOS for SimpleLink Wireless MCUs
2.14.03.28
|
UART driver implementation for a CC3200 UART controller, using the micro DMA controller.
============================================================================
The UART header file should be included in an application as follows:
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/ports/ClockP.h>
#include <ti/drivers/ports/HwiP.h>
#include <ti/drivers/ports/SemaphoreP.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/UART.h>
Go to the source code of this file.
Data Structures | |
struct | UARTCC3200DMA_HWAttrs |
UARTCC3200DMA Hardware attributes. More... | |
struct | UARTCC3200DMA_Object |
UARTCC3200DMA Object. More... | |
Typedefs | |
typedef struct UARTCC3200DMA_HWAttrs | UARTCC3200DMA_HWAttrs |
UARTCC3200DMA Hardware attributes. More... | |
typedef struct UARTCC3200DMA_Object | UARTCC3200DMA_Object |
UARTCC3200DMA Object. More... | |
typedef struct UARTCC3200DMA_Object * | UARTCC3200DMA_Handle |
Variables | |
const UART_FxnTable | UARTCC3200DMA_fxnTable |
typedef struct UARTCC3200DMA_HWAttrs UARTCC3200DMA_HWAttrs |
UARTCC3200DMA Hardware attributes.
These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For CC3200Ware these definitions are found in:
intPriority is the UART peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
A sample structure is shown below:
typedef struct UARTCC3200DMA_Object UARTCC3200DMA_Object |
UARTCC3200DMA Object.
The application must not access any member variables of this structure!
typedef struct UARTCC3200DMA_Object * UARTCC3200DMA_Handle |
const UART_FxnTable UARTCC3200DMA_fxnTable |