![]() |
![]() |
TI-RTOS for SimpleLink Wireless MCUs
2.14.03.28
|
UART driver implementation for a CC3200 UART controller.
============================================================================
The UARTCC3200 driver is (ring) buffered driver where it stores data it may already received in a user-supplied background buffer.
While permitted, it is STRONGLY suggested to avoid implementations where you call UART_read() within it own callback function (when in UART_MODE_CALLBACK).
Doing so, will require additional (task and system) stack for each nested UART_read() call.
Tool chain | Number of bytes per nested UART_read() call |
---|---|
GNU | 96 bytes + callback function stack requirements |
IAR | 40 bytes + callback function stack requirements |
TI | 80 bytes + callback function stack requirements |
It is important to note a potential worst case scenario: A full ring buffer with data; say 32 bytes The callback function calls UART_read() with a size of 1 (byte) No other variables are allocated in the callback function No other function calls are made in the callback function
As a result, you need an additional task and system stack of: 32 bytes * (80 bytes for TI + 0 bytes by the callback function) = 2.5kB
The UART header file should be included in an application as follows:
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/ports/ClockP.h>
#include <ti/drivers/ports/HwiP.h>
#include <ti/drivers/ports/SemaphoreP.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/UART.h>
#include <ti/drivers/uart/RingBuf.h>
Go to the source code of this file.
Data Structures | |
struct | UARTCC3200_FxnSet |
Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only. More... | |
struct | UARTCC3200_HWAttrs |
UARTCC3200 Hardware attributes. More... | |
struct | UARTCC3200_Object |
UARTCC3200 Object. More... | |
Typedefs | |
typedef struct UARTCC3200_FxnSet | UARTCC3200_FxnSet |
Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only. More... | |
typedef struct UARTCC3200_HWAttrs | UARTCC3200_HWAttrs |
UARTCC3200 Hardware attributes. More... | |
typedef struct UARTCC3200_Object | UARTCC3200_Object |
UARTCC3200 Object. More... | |
typedef struct UARTCC3200_Object * | UARTCC3200_Handle |
Variables | |
const UART_FxnTable | UARTCC3200_fxnTable |
typedef struct UARTCC3200_FxnSet UARTCC3200_FxnSet |
Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only.
These functions should not be used by the user and are solely intended for the UARTCC3200 driver. The UARTCC3200_FxnSet is a pair of complement functions that are design to operate with one another in a task context and in an ISR context. The readTaskFxn is called by UARTCC3200_read() to drain a circular buffer, whereas the readIsrFxn is used by the UARTCC3200_hwiIntFxn to fill up the circular buffer.
readTaskFxn: Function called by UART read These variables are set and avilalable for use to the readTaskFxn. object->readBuf = buffer; //Pointer to a user buffer object->readSize = size; //Desired no. of bytes to read object->readCount = size; //Remaining no. of bytes to read
readIsrFxn: The required ISR counterpart to readTaskFxn
typedef struct UARTCC3200_HWAttrs UARTCC3200_HWAttrs |
UARTCC3200 Hardware attributes.
The fields, baseAddr, intNum, and flowControl, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For CC3200Ware these definitions are found in:
intPriority is the UART peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
A sample structure is shown below:
typedef struct UARTCC3200_Object UARTCC3200_Object |
UARTCC3200 Object.
The application must not access any member variables of this structure!
typedef struct UARTCC3200_Object * UARTCC3200_Handle |
const UART_FxnTable UARTCC3200_fxnTable |