![]() |
![]() |
IPC API
3.40.00.06
|
Factory virtual function table. More...
#include <Ipc.h>
Data Fields | |
Int(* | createFxn )(Void) |
Void(* | deleteFxn )(Void) |
Int(* | attachFxn )(UInt16 procId) |
Int(* | detachFxn )(UInt16 procId) |
Factory virtual function table.
This virtual function table defines the interface which must be implemented by the transport factory. The Ipc module will use this factory to create and delete this transport. The factory is responsible for managing the details of creation and deletion.
Int(* Ipc_TransportFactoryFxns::createFxn) (Void) |
factory create method
Void(* Ipc_TransportFactoryFxns::deleteFxn) (Void) |
factory finalize method
Int(* Ipc_TransportFactoryFxns::attachFxn) (UInt16 procId) |
attach transport to processor
Int(* Ipc_TransportFactoryFxns::detachFxn) (UInt16 procId) |
detach transport from processor