IPC API  3.10.02.13
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Data Fields
MmRpc_Xlt Struct Reference

#include <MmRpc.h>

Collaboration diagram for MmRpc_Xlt:
Collaboration graph

Data Fields

uint32_t index
ptrdiff_t offset
size_t base
size_t handle

Field Documentation

uint32_t MmRpc_Xlt::index

parameter index to base pointer

ptrdiff_t MmRpc_Xlt::offset

offset to embedded pointer

                        If param type is MmRpc_ParamType_Ptr, offset
                        to embedded pointer from addr. If param type
                        is MmRpc_ParamType_OffPtr, offset to embedded
                        pointer from base+offset.
size_t MmRpc_Xlt::base

addr or file descriptor [+ data offset]

                        If param type is MmRpc_ParamType_Ptr, the
                        value of the embedded pointer. If param type
                        is MmRpc_ParamType_OffPtr, the file descriptor
                        of the block referenced by the embedded pointer
                        plus an optional data offset.
size_t MmRpc_Xlt::handle

memory allocator handle


The documentation for this struct was generated from the following file:
Copyright 2013, Texas Instruments Incorporated