![]() |
![]() |
IPC API
3.10.02.13
|
![]() ![]() | |
![]() ![]() ![]() | |
![]() ![]() ![]() ![]() | Remote Command Message Client Module. An RcmClient is used for sending messages to an RcmServer for processing |
![]() ![]() ![]() ![]() | Remote Command Message Server Module. An RcmServer processes inbound messages received from an RcmClient |
![]() ![]() ![]() ![]() | Remote Command Message Types |
![]() ![]() ![]() | |
![]() ![]() ![]() ![]() | |
![]() ![]() ![]() ![]() ![]() | Multi-Media derived Remote Procedure Call |
![]() ![]() ![]() ![]() ![]() | Multi-Media Service Manager |
![]() ![]() ![]() ![]() ![]() | Specific types to support the MmRpc and MmServiceMgr modules |
![]() ![]() ![]() ![]() | |
![]() ![]() ![]() ![]() ![]() | |
![]() ![]() ![]() ![]() ![]() | |
![]() ![]() ![]() ![]() ![]() | Example of a host-side module which uses MmRpc to invoke functions on a remote processor |
![]() ![]() ![]() ![]() ![]() | Example of a slave-side module which implements the Mx module functions. The functions in MxServer are invoked remotely by the Mx module running on the host processor |
![]() ![]() ![]() ![]() | Multiple processor gate that provides local and remote context protection |
![]() ![]() ![]() ![]() | Multi-processor fixed-size buffer heap implementation |
![]() ![]() ![]() ![]() | Multi-processor variable size buffer heap implementation |
![]() ![]() ![]() ![]() | Multiple fixed size buffer heap implementation |
![]() ![]() ![]() ![]() | Ipc Manager |
![]() ![]() ![]() ![]() | Multiple processor shared memory list |
![]() ![]() ![]() ![]() | MessageQ Manager |
![]() ![]() ![]() ![]() | Processor ID Manager |
![]() ![]() ![]() ![]() | NameServer Manager |
![]() ![]() ![]() ![]() | Notification manager for IPC |
![]() ![]() ![]() ![]() | Shared memory manager and address translator |