![]() |
![]() |
IPC API
3.10.02.13
|
Multi-processor variable size buffer heap implementation.
HeapMemMP is a heap implementation that manages variable size buffers that can be used in a multiprocessor system with shared memory. HeapMemMP manages a single buffer in shared memory from which blocks of user- specified length are allocated and freed.
The HeapMemMP module uses a NameServer instance to store instance information when an instance is created. The name supplied must be unique for all HeapMemMP instances.
HeapMemMP_create() initializes the shared memory as needed. Once an instance is created, HeapMemMP_open() can be called. The open is used to gain access to the same HeapMemMP instance. Generally an instance is created on one processor and opened on the other processor(s).
The open returns a HeapMemMP instance handle like the create, however the open does not modify the shared memory.
Because HeapMemMP is a variable-size heap implementation, it is also used by the SharedRegion module to manage shared memory in each shared region. When any shared memory IPC instance is created in a particular shared region, the HeapMemMP that manages shared memory in the shared region allocates shared memory for the instance.
The HeapMemMP header should be included in an application as follows:
#include <ti/ipc/GateMP.h>
Go to the source code of this file.
Data Structures | |
struct | HeapMemMP_Params |
Structure defining parameters for the HeapMemMP module. More... | |
struct | HeapMemMP_ExtendedStats |
Stats structure for HeapMemMP_getExtendedStats() More... |
Macros | |
#define | HeapMemMP_S_BUSY 2 |
The resource is still in use. | |
#define | HeapMemMP_S_ALREADYSETUP 1 |
The module has been already setup. | |
#define | HeapMemMP_S_SUCCESS 0 |
Operation is successful. | |
#define | HeapMemMP_E_FAIL -1 |
Generic failure. | |
#define | HeapMemMP_E_INVALIDARG -2 |
Argument passed to function is invalid. | |
#define | HeapMemMP_E_MEMORY -3 |
Operation resulted in memory failure. | |
#define | HeapMemMP_E_ALREADYEXISTS -4 |
The specified entity already exists. | |
#define | HeapMemMP_E_NOTFOUND -5 |
Unable to find the specified entity. | |
#define | HeapMemMP_E_TIMEOUT -6 |
Operation timed out. | |
#define | HeapMemMP_E_INVALIDSTATE -7 |
Module is not initialized. | |
#define | HeapMemMP_E_OSFAILURE -8 |
A failure occurred in an OS-specific call. | |
#define | HeapMemMP_E_RESOURCE -9 |
Specified resource is not available. | |
#define | HeapMemMP_E_RESTART -10 |
Operation was interrupted. Please restart the operation. |
Typedefs | |
typedef struct HeapMemMP_Object * | HeapMemMP_Handle |
HeapMemMP_Handle type. | |
typedef struct HeapMemMP_Params | HeapMemMP_Params |
Structure defining parameters for the HeapMemMP module. | |
typedef struct HeapMemMP_ExtendedStats | HeapMemMP_ExtendedStats |
Stats structure for HeapMemMP_getExtendedStats() |
Functions | |
Int | HeapMemMP_close (HeapMemMP_Handle *handlePtr) |
Close a HeapMemMP instance. | |
HeapMemMP_Handle | HeapMemMP_create (const HeapMemMP_Params *params) |
Create a HeapMemMP instance. | |
Int | HeapMemMP_delete (HeapMemMP_Handle *handlePtr) |
Delete a created HeapMemMP instance. | |
Int | HeapMemMP_open (String name, HeapMemMP_Handle *handlePtr) |
Open a created HeapMemMP instance. | |
Void | HeapMemMP_Params_init (HeapMemMP_Params *params) |
Initialize a HeapMemMP parameters struct. | |
Void * | HeapMemMP_alloc (HeapMemMP_Handle handle, SizeT size, SizeT align) |
Allocate a block of memory of specified size and alignment. | |
Void | HeapMemMP_free (HeapMemMP_Handle handle, Ptr block, SizeT size) |
Frees a block of memory. | |
Void | HeapMemMP_getExtendedStats (HeapMemMP_Handle handle, HeapMemMP_ExtendedStats *stats) |
Get extended memory statistics. | |
Void | HeapMemMP_getStats (HeapMemMP_Handle handle, Ptr stats) |
Get memory statistics. | |
Void | HeapMemMP_restore (HeapMemMP_Handle handle) |
Restore an instance to it's original created state. |
#define HeapMemMP_S_BUSY 2 |
The resource is still in use.
#define HeapMemMP_S_ALREADYSETUP 1 |
The module has been already setup.
#define HeapMemMP_S_SUCCESS 0 |
Operation is successful.
#define HeapMemMP_E_FAIL -1 |
Generic failure.
#define HeapMemMP_E_INVALIDARG -2 |
Argument passed to function is invalid.
#define HeapMemMP_E_MEMORY -3 |
Operation resulted in memory failure.
#define HeapMemMP_E_ALREADYEXISTS -4 |
The specified entity already exists.
#define HeapMemMP_E_NOTFOUND -5 |
Unable to find the specified entity.
#define HeapMemMP_E_TIMEOUT -6 |
Operation timed out.
#define HeapMemMP_E_INVALIDSTATE -7 |
Module is not initialized.
#define HeapMemMP_E_OSFAILURE -8 |
A failure occurred in an OS-specific call.
#define HeapMemMP_E_RESOURCE -9 |
Specified resource is not available.
#define HeapMemMP_E_RESTART -10 |
Operation was interrupted. Please restart the operation.
typedef struct HeapMemMP_Object* HeapMemMP_Handle |
HeapMemMP_Handle type.
typedef struct HeapMemMP_Params HeapMemMP_Params |
Structure defining parameters for the HeapMemMP module.
typedef struct HeapMemMP_ExtendedStats HeapMemMP_ExtendedStats |
Stats structure for HeapMemMP_getExtendedStats()
Int HeapMemMP_close | ( | HeapMemMP_Handle * | handlePtr | ) |
Close a HeapMemMP instance.
Closing an instance will free local memory consumed by the opened instance. All opened instances should be closed before the instance is deleted.
[in,out] | handlePtr | Pointer to handle returned from HeapMemMP_open() |
HeapMemMP_Handle HeapMemMP_create | ( | const HeapMemMP_Params * | params | ) |
Create a HeapMemMP instance.
[in] | params | HeapMemMP parameters |
Int HeapMemMP_delete | ( | HeapMemMP_Handle * | handlePtr | ) |
Delete a created HeapMemMP instance.
[in,out] | handlePtr | Pointer to handle to delete. |
Int HeapMemMP_open | ( | String | name, |
HeapMemMP_Handle * | handlePtr | ||
) |
Open a created HeapMemMP instance.
Once an instance is created, an open can be performed. The open is used to gain access to the same HeapMemMP instance. Generally an instance is created on one processor and opened on the other processor.
The open returns a HeapMemMP instance handle like the create, however the open does not initialize the shared memory. The supplied name is used to identify the created instance.
Call HeapMemMP_close when the opened instance is not longer needed.
[in] | name | Name of created HeapMemMP instance |
[out] | handlePtr | Pointer to HeapMemMP handle to be opened |
Void HeapMemMP_Params_init | ( | HeapMemMP_Params * | params | ) |
Initialize a HeapMemMP parameters struct.
[out] | params | Pointer to creation parameters |
Void* HeapMemMP_alloc | ( | HeapMemMP_Handle | handle, |
SizeT | size, | ||
SizeT | align | ||
) |
Allocate a block of memory of specified size and alignment.
The actual block returned may be larger than requested to satisfy alignment requirements. NULL is returned if the alloc fails.
HeapMemMP_alloc will lock the heap using the HeapMemMP gate while it traverses the list of free blocks to find a large enough block for the request.
Guidelines for using large heaps and multiple alloc() calls.
[in] | handle | Handle to previously created/opened instance. |
[in] | size | Size to be allocated (in MADUs) |
[in] | align | Alignment for allocation (power of 2) |
Void HeapMemMP_free | ( | HeapMemMP_Handle | handle, |
Ptr | block, | ||
SizeT | size | ||
) |
Frees a block of memory.
HeapMemMP_free() places the memory block specified by addr and size back into the free pool of the heap specified. The newly freed block is combined with any adjacent free blocks. The space is then available for future allocations.
HeapMemMP_free() will lock the heap using the HeapMemMP gate if one is specified or the system GateMP if not.
[in] | handle | Handle to previously created/opened instance. |
[in] | block | Block of memory to be freed. |
[in] | size | Size to be freed (in MADUs) |
Void HeapMemMP_getExtendedStats | ( | HeapMemMP_Handle | handle, |
HeapMemMP_ExtendedStats * | stats | ||
) |
Get extended memory statistics.
This function retrieves extended statistics for a HeapMemMP instance. Refer to HeapMemMP_ExtendedStats for more information regarding what information is returned.
[in] | handle | Handle to previously created/opened instance. |
[out] | stats | ExtendedStats structure |
Void HeapMemMP_getStats | ( | HeapMemMP_Handle | handle, |
Ptr | stats | ||
) |
Get memory statistics.
[in] | handle | Handle to previously created/opened instance. |
[out] | stats | Memory statistics structure |
Void HeapMemMP_restore | ( | HeapMemMP_Handle | handle | ) |
Restore an instance to it's original created state.
This function restores an instance to its original created state. Any memory previously allocated from the heap is no longer valid after this API is called. This function does not check whether there is allocated memory or not.
[in] | handle | Handle to previously created/opened instance. |