![]() |
![]() |
IPC API
3.00.03.28
|
![]() ![]() | Structure defining parameters for the GateMP module |
![]() ![]() | Stats structure for HeapBufMP_getExtendedStats() |
![]() ![]() | Structure defining parameters for the HeapBufMP module |
![]() ![]() | Stats structure for HeapMemMP_getExtendedStats() |
![]() ![]() | Structure defining parameters for the HeapMemMP module |
![]() ![]() | Structure for bucket configuration |
![]() ![]() | Stats structure for the HeapMultiBufMP_getExtendedStats() API |
![]() ![]() | Structure defining parameters for the HeapMultiBufMP module |
![]() ![]() | Structure defining a ListMP element |
![]() ![]() | Structure defining parameter structure for ListMP_create() |
![]() ![]() | Required first field in every message |
![]() ![]() | Structure defining parameters for the MessageQ module |
![]() ![]() | Function call context structure |
![]() ![]() | MmRpc_Param type |
![]() ![]() | Instance create parameters |
![]() ![]() | |
![]() ![]() | Function Signature |
![]() ![]() | Function Signature Table |
![]() ![]() | Marshalled Parameter structure |
![]() ![]() | Parameter Signature |
![]() ![]() | Compute structure |
![]() ![]() | Compute structure |
![]() ![]() | NameServer_Handle type |
![]() ![]() | Remote Command Message structure |
![]() ![]() | |
![]() ![]() | Instance create parameters |
![]() ![]() | Opaque client structure large enough to hold an instance object |
![]() ![]() | Function descriptor |
![]() ![]() | Function descriptor array |
![]() ![]() | RcmServer Instance create parameters |
![]() ![]() | Worker pool descriptor |
![]() ![]() | Worker pool descriptor array |
![]() ![]() | |
![]() ![]() | Structure defining a region |