module ti.sdo.ipc.transports.TransportShmNotifySetup |
|
|
|
Manages the setup of TransportShmNotify instances
create or open the TransportShmNotify for each pair of devices.
#include <ti/sdo/ipc/transports/TransportShmNotifySetup.h>
Functions common to all ITransportSetup modules |
Int | |
Int | |
Bool | |
SizeT | |
Functions common to all target modules |
|
|
Constants |
extern const UInt | |
config TransportShmNotifySetup_priority // module-wide |
|
priority of the transport
extern const UInt TransportShmNotifySetup_priority;
TransportShmNotifySetup_attach() // module-wide |
|
Function that will be called in MessageQ_attach
Int TransportShmNotifySetup_attach(UInt16 remoteProcId, Ptr sharedAddr);
TransportShmNotifySetup_detach() // module-wide |
|
Function that will be called in MessageQ_detach
Int TransportShmNotifySetup_detach(UInt16 remoteProcId);
TransportShmNotifySetup_isRegistered() // module-wide |
|
Determines if a transport has been registered to a remote processor
Bool TransportShmNotifySetup_isRegistered(UInt16 remoteProcId);
TransportShmNotifySetup_sharedMemReq() // module-wide |
|
Shared memory required
SizeT TransportShmNotifySetup_sharedMemReq(Ptr sharedAddr);
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool TransportShmNotifySetup_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool TransportShmNotifySetup_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 TransportShmNotifySetup_Module_getMask();
// Returns the diagnostics mask for this module
Void TransportShmNotifySetup_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var TransportShmNotifySetup = xdc.useModule('ti.sdo.ipc.transports.TransportShmNotifySetup');
module-wide config parameters
generated on Sat, 11 Feb 2012 00:38:12 GMT