![]() |
![]() |
Framework Components Application Programming Interface (API)
fc-v07
|
IRES_TILEDMEMORY_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More...
#include <ires_tiledmemory.h>
Data Fields | |
IRES_Obj | ires |
XDAS_Void * | info |
XDAS_Void * | memoryBaseAddress |
XDAS_UInt32 | isTiledMemory |
XDAS_UInt32 | accessUnit |
XDAS_Void * | tilerBaseAddress |
XDAS_Void * | systemSpaceBaseAddress |
IRES_TILEDMEMORY_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.
IRES_Obj IRES_TILEDMEMORY_Obj::ires |
XDAS_Void* IRES_TILEDMEMORY_Obj::info |
RSVD for future use
XDAS_Void* IRES_TILEDMEMORY_Obj::memoryBaseAddress |
Process-specific virtual base address of Tiler memory allocated.
XDAS_UInt32 IRES_TILEDMEMORY_Obj::isTiledMemory |
Boolean value that identifies if returned memory is of type TILED memory or not.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
If XDAS_TRUE, accessUnit will describe the kind of TILED memory allocated.
XDAS_UInt32 IRES_TILEDMEMORY_Obj::accessUnit |
Describes the kind of memory actually allocated in the TILER space of type,
XDAS_Void* IRES_TILEDMEMORY_Obj::tilerBaseAddress |
Base address of TILER on SOC
XDAS_Void* IRES_TILEDMEMORY_Obj::systemSpaceBaseAddress |
Tiler space base address of memory allocated