![]() |
![]() |
Configuration Parameters required by the Resource Manager implementation. These can be extended by individual resource managers if required. More...
#include <iresman.h>
Data Fields | |
Int32 | size |
Size of the structure. | |
IRESMAN_PersistentAllocFxn * | allocFxn |
Function to allocate memory required by the resource manager implementation and the protocol. | |
IRESMAN_PersistentFreeFxn * | freeFxn |
Function to free memory released by the resource manager implementation and the protocol. |
Configuration Parameters required by the Resource Manager implementation. These can be extended by individual resource managers if required.
Int32 IRESMAN_Params::size |
Size of the structure.
Function to allocate memory required by the resource manager implementation and the protocol.
Function to free memory released by the resource manager implementation and the protocol.