Resource manager interface
Data Structures |
struct | IRESMAN_Params |
| Configuration Parameters required by the Resource Manager implementation. These can be extended by individual resource managers if required. More...
|
struct | IRESMAN_Fxns |
struct | IRESMAN_ConstructArgs |
| Abstract Protocol Construct Arguments structure/pointer definition. Arguments passed by the Resource manager to request a resource from a specific IRES Protocol will extend and supply the concrete definition. More...
|
Typedefs |
typedef Bool( | IRESMAN_PersistentAllocFxn )(IALG_MemRec *memTab, Int numRecs) |
| Memory allocation function for all of ResMan and other IRES protocol's memory requirements.
|
typedef Void( | IRESMAN_PersistentFreeFxn )(IALG_MemRec *memTab, Int numRecs) |
| Memory free functions for all of ResMan and other IRES protocol's memory requirements.
|
Detailed Description
The IRESMAN interface needs to be implemented and registered with the generic RMAN Resource Registry and is called by the Framework resource manager (RMAN) to manage corresponding IRES resources
Typedef Documentation
Memory allocation function for all of ResMan and other IRES protocol's memory requirements.
Memory free functions for all of ResMan and other IRES protocol's memory requirements.