![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Descriptor for the chunk of data being transferred in one call to putData or getData. More...
#include <xdm.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | scatteredBlocksFlag |
XDAS_Int32 * | baseAddr |
XDAS_Int32 | numBlocks |
XDAS_Int32 | varBlockSizesFlag |
XDAS_Int32 * | blockSizes |
Descriptor for the chunk of data being transferred in one call to putData or getData.
XDAS_Int32 XDM_DataSyncDesc::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 XDM_DataSyncDesc::scatteredBlocksFlag |
Flag indicating whether the individual data blocks may be scattered in memory.
baseAddr
field points directly to the start of the first block, and is not treated as a pointer to an array.baseAddr
array must contain the base address of each individual block. XDAS_Int32* XDM_DataSyncDesc::baseAddr |
Base address of single data block or pointer to an array of data block addresses of size numBlocks
.
scatteredBlocksFlag
is set to XDAS_FALSE, this field points directly to the start of the first block, and is not treated as a pointer to an array.scatteredBlocksFlag
is set to XDAS_TRUE, this field points to an array of pointers to the data blocks. XDAS_Int32 XDM_DataSyncDesc::numBlocks |
Number of blocks available
XDAS_Int32 XDM_DataSyncDesc::varBlockSizesFlag |
Flag indicating whether any of the data blocks vary in size.
XDAS_Int32* XDM_DataSyncDesc::blockSizes |
Variable block sizes array.
@remarks If @c varBlockSizesFlag is XDAS_TRUE, this array contains the sizes of each block. If @c varBlockSizesFlag is XDAS_FALSE, this contains the size of same-size blocks. @remarks Memory for this array (of size @c numBlocks) has to be allocated by the caller of the putData API.