Codec Engine Application Programming Interface (API)
ce-w08
|
Defines the input arguments for all IVIDTRANSCODE instance process function. More...
#include <ividtranscode.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numBytes |
XDAS_Int32 | inputID |
Defines the input arguments for all IVIDTRANSCODE instance process function.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IVIDTRANSCODE_Fxns::process()
XDAS_Int32 IVIDTRANSCODE_InArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDTRANSCODE_InArgs::numBytes |
Size of input data in bytes, provided to the algorithm for decoding.
XDAS_Int32 IVIDTRANSCODE_InArgs::inputID |
The decoder will attach this ID with the corresponding output frames.