![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Detailed buffer descriptor for video buffers. More...
#include <ivideo.h>
Data Fields | |
XDAS_Int32 | numBufs |
XDAS_Int32 | frameWidth |
XDAS_Int32 | frameHeight |
XDAS_Int32 | framePitch |
XDM1_SingleBufDesc | bufDesc [3] |
XDAS_Int32 | extendedError |
Extended error information. | |
XDAS_Int32 | frameType |
Video frame types. | |
XDAS_Int32 | topFieldFirstFlag |
XDAS_Int32 | repeatFirstFieldFlag |
XDAS_Int32 | frameStatus |
Video output buffer status. | |
XDAS_Int32 | repeatFrame |
XDAS_Int32 | contentType |
XDAS_Int32 | chromaFormat |
Chroma formats. |
Detailed buffer descriptor for video buffers.
XDAS_Int32 IVIDEO1_BufDesc::numBufs |
Number of buffers in bufDesc[].
XDAS_Int32 IVIDEO1_BufDesc::frameWidth |
Width of the video frame.
XDAS_Int32 IVIDEO1_BufDesc::frameHeight |
Height of the video frame.
XDAS_Int32 IVIDEO1_BufDesc::framePitch |
Frame pitch used to store the frame.
@remarks This field can also be used to indicate the padded width.
XDM1_SingleBufDesc IVIDEO1_BufDesc::bufDesc[3] |
Picture buffers.
XDAS_Int32 IVIDEO1_BufDesc::extendedError |
Extended error information.
XDAS_Int32 IVIDEO1_BufDesc::frameType |
Video frame types.
@remarks For the various @c IVIDEO_xy_FRAME values, this frame type is interlaced where both top and bottom fields are provided in a single frame. The first field is an "x" frame, the second field is "y" field. @remarks This enumeration data type should not be used for storage, but rather only for its constant values. @remarks This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between #XDM_CUSTOMENUMBASE and 0x7FFF.
@sa IVIDEO_FrameType
XDAS_Int32 IVIDEO1_BufDesc::topFieldFirstFlag |
Flag to indicate when the application should display the top field first.
XDAS_Int32 IVIDEO1_BufDesc::repeatFirstFieldFlag |
Flag to indicate when the first field should be repeated.
XDAS_Int32 IVIDEO1_BufDesc::frameStatus |
Video output buffer status.
@remarks Ownership of the buffers, either by application or algorithm, is conveyed via these values. @remarks This reflects the status of ALL output buffers. For example, if video decoded output is in 4:2:0 format, all the 3 output buffers' status is described by this value. Similarly, for 4:2:2 formatted buffers, this value describes the single buffer's status. @remarks This enumeration data type should not be used for storage, but rather only for its constant values. @remarks This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between #XDM_CUSTOMENUMBASE and 0x7FFF.
@sa IVIDEO_OutputFrameStatus @remarks This field does not apply to encoder recon bufs.
XDAS_Int32 IVIDEO1_BufDesc::repeatFrame |
Number of times the display process needs to repeat the displayed progressive frame.
XDAS_Int32 IVIDEO1_BufDesc::contentType |
Content type of the buffer.
@remarks This is useful when the content is both interlaced and progressive. The display process can use this field to determine how to render the display buffer. @sa IVIDEO_ContentType
XDAS_Int32 IVIDEO1_BufDesc::chromaFormat |
Chroma formats.
@remarks This enumeration data type should not be used for storage, but rather only for its constant values. @remarks This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between #XDM_CUSTOMENUMBASE and 0x7FFF.
@sa XDM_ChromaFormat