![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines the run time output arguments for all IVIDENC2 instance objects. More...
#include <ividenc2.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
Extended error information. | |
XDAS_Int32 | bytesGenerated |
XDAS_Int32 | encodedFrameType |
Video frame types. | |
XDAS_Int32 | inputFrameSkip |
Video frame skipping modes. | |
XDAS_Int32 | freeBufID [20] |
IVIDEO2_BufDesc | reconBufs |
Defines the run time output arguments for all IVIDENC2 instance objects.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IVIDENC2_Fxns::process()
XDAS_Int32 IVIDENC2_OutArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDENC2_OutArgs::extendedError |
Extended error information.
XDAS_Int32 IVIDENC2_OutArgs::bytesGenerated |
Number of bytes generated during the IVIDENC2_Fxns::process() call.
XDAS_Int32 IVIDENC2_OutArgs::encodedFrameType |
Video frame types.
@remarks For the various @c IVIDEO_xy_FRAME values, this frame type is interlaced where both top and bottom fields are provided in a single frame. The first field is an "x" frame, the second field is "y" field. @remarks This enumeration data type should not be used for storage, but rather only for its constant values. @remarks This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between #XDM_CUSTOMENUMBASE and 0x7FFF.
@sa IVIDEO_FrameType
XDAS_Int32 IVIDENC2_OutArgs::inputFrameSkip |
Video frame skipping modes.
@remarks This enumeration data type should not be used for storage, but rather only for its constant values. @remarks This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between #XDM_CUSTOMENUMBASE and 0x7FFF.
@sa IVIDEO_SkipMode
XDAS_Int32 IVIDENC2_OutArgs::freeBufID[20] |
This is an array of inputID's corresponding to the buffers that have been unlocked in the current process call.
freeBufID
[0] will have a value of zero.IVIDEO2_BufDesc IVIDENC2_OutArgs::reconBufs |
Reconstruction frames.