Codec Engine Application Programming Interface (API)
ce-w08
|
Defines the creation time parameters for all IVIDDEC instance objects. More...
#include <ividdec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxHeight |
XDAS_Int32 | maxWidth |
XDAS_Int32 | maxFrameRate |
XDAS_Int32 | maxBitRate |
XDAS_Int32 | dataEndianness |
XDAS_Int32 | forceChromaFormat |
Defines the creation time parameters for all IVIDDEC instance objects.
@remarks The application should set the parameters to 0 to use the algorithm's default values. @remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int32 IVIDDEC_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDDEC_Params::maxHeight |
Maximum video height in pixels.
XDAS_Int32 IVIDDEC_Params::maxWidth |
Maximum video width in pixels.
XDAS_Int32 IVIDDEC_Params::maxFrameRate |
Maximum frame rate in fps * 1000.
XDAS_Int32 IVIDDEC_Params::maxBitRate |
Maximum bit rate, bits per second. For example, if bit rate is 10 Mbps, set this field to 10000000
XDAS_Int32 IVIDDEC_Params::dataEndianness |
Endianness of input data.
@sa XDM_DataFormat
XDAS_Int32 IVIDDEC_Params::forceChromaFormat |
Force decode in given Chroma format.
@sa XDM_ChromaFormat