![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines instance status parameters. More...
#include <ividdec3.h>
Defines instance status parameters.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IVIDDEC3_Fxns::control()
XDAS_Int32 IVIDDEC3_Status::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDDEC3_Status::extendedError |
Extended error information.
XDM1_SingleBufDesc IVIDDEC3_Status::data |
Buffer descriptor for data passing.
@remarks If this field is not used, the application <b>must</b> set @c data.buf to NULL. @remarks This buffer can be used as either input or output, depending on the command. @remarks The buffer will be provided by the application, and returned to the application upon return of the IVIDDEC3_Fxns.control() call. The algorithm must not retain a pointer to this data. @sa #XDM_GETVERSION
XDAS_Int32 IVIDDEC3_Status::maxNumDisplayBufs |
The maximum number of buffers that will be required by the codec.
XDAS_Int32 IVIDDEC3_Status::maxOutArgsDisplayBufs |
The maximum number of display buffers that can be returned via IVIDDEC3_OutArgs.displayBufs.
XDAS_Int32 IVIDDEC3_Status::outputHeight |
Output height in pixels.
XDAS_Int32 IVIDDEC3_Status::outputWidth |
Output width in pixels.
XDAS_Int32 IVIDDEC3_Status::frameRate |
Average frame rate in fps * 1000. For example, if average frame rate is 30 frames per second, this field should be 30000.
XDAS_Int32 IVIDDEC3_Status::bitRate |
Average bit rate, in bits per second.
XDAS_Int32 IVIDDEC3_Status::contentType |
Video content types.
@remarks This enumeration data type should not be used for storage, but rather only for its constant values. @remarks This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between #XDM_CUSTOMENUMBASE and 0x7FFF.
@sa IVIDEO_ContentType
XDAS_Int32 IVIDDEC3_Status::sampleAspectRatioHeight |
Sample aspect ratio height.
XDAS_Int32 IVIDDEC3_Status::sampleAspectRatioWidth |
Sample aspect ratio width.
XDAS_Int32 IVIDDEC3_Status::bitRange |
Full 8 bit, CCIR 601
XDAS_Int32 IVIDDEC3_Status::forceChromaFormat |
Output chroma format.
@sa XDM_ChromaFormat
XDAS_Int32 IVIDDEC3_Status::operatingMode |
Video decoding mode of operation.
@sa IVIDEO_OperatingMode
XDAS_Int32 IVIDDEC3_Status::frameOrder |
Frame Order
@remarks This field reflects the value provided during creation in IVIDDEC3_Params.displayDelay
XDAS_Int32 IVIDDEC3_Status::inputDataMode |
Input data mode.
@sa IVIDDEC3_Params.inputDataMode @sa IVIDEO_DataMode
XDAS_Int32 IVIDDEC3_Status::outputDataMode |
Output data mode.
@sa IVIDDEC3_Params.outputDataMode @sa IVIDEO_DataMode
XDM1_AlgBufInfo IVIDDEC3_Status::bufInfo |
Input and output buffer information.
@remarks This field provides the application with the algorithm's buffer requirements. The requirements may vary depending on the current configuration of the algorithm instance. @sa XDM1_AlgBufInfo
XDAS_Int32 IVIDDEC3_Status::numInputDataUnits |
Number of input slices/rows.
@remarks Units depend on the IVIDDEC3_Params.inputDataMode, like number of slices/rows/blocks etc. @remarks Ignored if IVIDDEC3_Params.inputDataMode is set to full frame mode. @sa IVIDDEC3_Params.inputDataMode
XDAS_Int32 IVIDDEC3_Status::numOutputDataUnits |
Number of output slices/rows.
@remarks Units depend on the @c outputDataMode, like number of slices/rows/blocks etc. @remarks Ignored if IVIDDEC3_Params.outputDataMode is set to full frame mode. @sa IVIDDEC3_Params.outputDataMode
XDAS_Int32 IVIDDEC3_Status::configurationID |
Configuration ID of given codec.
@remarks This is based on the input stream & can be used by the framework to optimize the save/restore overhead of any resources used. @remarks This can be useful in multichannel use case scenarios.
XDAS_Int32 IVIDDEC3_Status::metadataType[3] |
Type of each metadata plane.
IVIDDEC3_DynamicParams IVIDDEC3_Status::decDynamicParams |
Current values of the decoder's dynamic parameters.