![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines the creation time parameters for all IVIDDEC3 instance objects. More...
#include <ividdec3.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxHeight |
XDAS_Int32 | maxWidth |
XDAS_Int32 | maxFrameRate |
XDAS_Int32 | maxBitRate |
XDAS_Int32 | dataEndianness |
XDAS_Int32 | forceChromaFormat |
Chroma formats. | |
XDAS_Int32 | operatingMode |
XDAS_Int32 | displayDelay |
Video decoder output frame order. | |
XDAS_Int32 | inputDataMode |
XDAS_Int32 | outputDataMode |
XDAS_Int32 | numInputDataUnits |
XDAS_Int32 | numOutputDataUnits |
XDAS_Int32 | errorInfoMode |
XDAS_Int32 | displayBufsMode |
XDAS_Int32 | metadataType [3] |
Defines the creation time parameters for all IVIDDEC3 instance objects.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int32 IVIDDEC3_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDDEC3_Params::maxHeight |
Maximum video height in pixels.
XDAS_Int32 IVIDDEC3_Params::maxWidth |
Maximum video width in pixels.
XDAS_Int32 IVIDDEC3_Params::maxFrameRate |
Maximum frame rate in fps * 1000. For example, if max frame rate is 30 frames per second, set this field to 30000.
XDAS_Int32 IVIDDEC3_Params::maxBitRate |
Maximum bit rate, bits per second. For example, if bit rate is 10 Mbps, set this field to 10000000
XDAS_Int32 IVIDDEC3_Params::dataEndianness |
Endianness of output data.
@sa XDM_DataFormat
XDAS_Int32 IVIDDEC3_Params::forceChromaFormat |
Chroma formats.
@remarks This enumeration data type should not be used for storage, but rather only for its constant values. @remarks This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between #XDM_CUSTOMENUMBASE and 0x7FFF.
@sa XDM_ChromaFormat
XDAS_Int32 IVIDDEC3_Params::operatingMode |
Video coding mode of operation.
@sa IVIDEO_OperatingMode
XDAS_Int32 IVIDDEC3_Params::displayDelay |
Video decoder output frame order.
@sa IVIDDEC3_displayDelay
XDAS_Int32 IVIDDEC3_Params::inputDataMode |
Input data mode.
@remarks If a subframe mode is provided, the application must call IVIDDEC3_Fxns.control() with #XDM_SETPARAMS id prior to IVIDDEC3_Fxns.process() to set IVIDDEC3_DynamicParams.getDataFxn() and IVIDDEC3_DynamicParams.getDataHandle (and optionally IVIDDEC3_DynamicParams.putBufferFxn(), and IVIDDEC3_DynamicParams.putBufferHandle). Else, the alg can return error. @sa IVIDEO_DataMode
XDAS_Int32 IVIDDEC3_Params::outputDataMode |
Output data mode.
@remarks If a subframe mode is provided, the application must call IVIDDEC3_Fxns.control() with #XDM_SETPARAMS id prior to #IVIDDEC3_Fxns.process() to set IVIDDEC3_DynamicParams.putDataFxn(), and IVIDDEC3_DynamicParams.putDataHandle. Else, the alg can return error. @sa IVIDEO_DataMode
XDAS_Int32 IVIDDEC3_Params::numInputDataUnits |
Number of input slices/rows.
@remarks Units depend on the IVIDDEC3_Params.inputDataMode, like number of slices/rows/blocks etc. @remarks Ignored if IVIDDEC3_Params.inputDataMode is set to full frame mode.
XDAS_Int32 IVIDDEC3_Params::numOutputDataUnits |
Number of output slices/rows.
@remarks Units depend on the IVIDDEC3_Params.outputDataMode, like number of slices/rows/blocks etc. @remarks Ignored if IVIDDEC3_Params.outputDataMode is set to full frame mode.
XDAS_Int32 IVIDDEC3_Params::errorInfoMode |
Enable/disable packet error information for input and/or output.
XDAS_Int32 IVIDDEC3_Params::displayBufsMode |
Indicates which mode the displayBufs are presented in.
XDAS_Int32 IVIDDEC3_Params::metadataType[3] |
Type of each metadata plane.