![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines instance status parameters. More...
#include <ividanalytics.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
Extended error information. | |
XDM1_BufDesc | data |
XDM_AlgBufInfo | bufInfo |
XDAS_Int32 | viewState |
View state of the analytics engine. |
Defines instance status parameters.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IVIDANALYTICS_Fxns::control()
XDAS_Int32 IVIDANALYTICS_Status::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDANALYTICS_Status::extendedError |
Extended error information.
XDM1_BufDesc IVIDANALYTICS_Status::data |
Buffer descriptors for data passing.
@remarks If this field is not used, the application <b>must</b> set @c data.numBufs to 0. @remarks These buffers can be used as either input or output, depending on the command. @remarks The buffers will be provided by the application, and returned to the application upon return of the IVIDANALYTICS_Fxns.control() call. The algorithm must not retain a pointer to this data. @sa #XDM_GETVERSION
XDM_AlgBufInfo IVIDANALYTICS_Status::bufInfo |
Input and output buffer information.
@remarks This field provides the application with the algorithm's buffer requirements. The requirements may vary depending on the current configuration of the algorithm instance. @sa IVIDANALYTICS_Params @sa XDM_AlgBufInfo @sa IVIDANALYTICS_Fxns::control()
XDAS_Int32 IVIDANALYTICS_Status::viewState |
View state of the analytics engine.
@sa IVIDANALYTICS_ViewState