![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines the run time output arguments for all ISPHDEC1 instance objects. More...
#include <isphdec1.h>
Data Fields | |
XDAS_Int16 | size |
XDAS_Int16 | dataSize |
XDAS_Int32 | extendedError |
Extended error information. |
Defines the run time output arguments for all ISPHDEC1 instance objects.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa ISPHDEC1_Fxns::process()
XDAS_Int16 ISPHDEC1_OutArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int16 ISPHDEC1_OutArgs::dataSize |
Size of raw data output in bits.
XDAS_Int32 ISPHDEC1_OutArgs::extendedError |
Extended error information.