![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines the creation time parameters for all IIMGDEC instance objects. More...
#include <iimgdec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxHeight |
XDAS_Int32 | maxWidth |
XDAS_Int32 | maxScans |
XDAS_Int32 | dataEndianness |
XDAS_Int32 | forceChromaFormat |
Chroma formats. |
Defines the creation time parameters for all IIMGDEC instance objects.
@remarks The application should set the parameters to 0 to use the algorithm's default values. @remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int32 IIMGDEC_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IIMGDEC_Params::maxHeight |
Maximum image height.
XDAS_Int32 IIMGDEC_Params::maxWidth |
Maximum image width.
XDAS_Int32 IIMGDEC_Params::maxScans |
Maximum number of scans.
XDAS_Int32 IIMGDEC_Params::dataEndianness |
Endianness of output data.
@sa XDM_DataFormat
XDAS_Int32 IIMGDEC_Params::forceChromaFormat |
Chroma formats.
@remarks This enumeration data type should not be used for storage, but rather only for its constant values. @remarks This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between #XDM_CUSTOMENUMBASE and 0x7FFF.
@sa XDM_ChromaFormat.