![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines the creation time parameters for all IAUDENC instance objects. More...
#include <iaudenc.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | encodingPreset |
XDAS_Int32 | maxSampleRate |
XDAS_Int32 | maxBitrate |
XDAS_Int32 | maxNoOfCh |
XDAS_Int32 | dataEndianness |
Defines the creation time parameters for all IAUDENC instance objects.
@remarks The application should set the parameters to 0 to use the algorithm's default values. @remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int32 IAUDENC_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IAUDENC_Params::encodingPreset |
Encoding Preset. See XDM_EncodingPreset.
XDAS_Int32 IAUDENC_Params::maxSampleRate |
Maximum sampling frequency in Hz. For example, if the maximum sampling frequency is 44.1 kHz, this field should be 44100.
XDAS_Int32 IAUDENC_Params::maxBitrate |
Maximum bit rate in bits per second. For example, if the maximum bit rate is 128 kbps, set this field to 128000.
XDAS_Int32 IAUDENC_Params::maxNoOfCh |
Maximum Channels. See IAUDIO_ChannelId.
XDAS_Int32 IAUDENC_Params::dataEndianness |
Endianness of output data.
@sa XDM_DataFormat