![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines instance status parameters (read-only). More...
#include <iauddec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
Extended error information. | |
XDAS_Int32 | bitRate |
XDAS_Int32 | sampleRate |
XDAS_Int32 | numChannels |
XDAS_Int32 | numLFEChannels |
XDAS_Int32 | outputFormat |
XDAS_Int32 | autoPosition |
XDAS_Int32 | fastFwdLen |
XDAS_Int32 | frameLen |
XDAS_Int32 | outputBitsPerSample |
XDM_AlgBufInfo | bufInfo |
Defines instance status parameters (read-only).
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IAUDDEC_Fxns::control()
XDAS_Int32 IAUDDEC_Status::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IAUDDEC_Status::extendedError |
Extended error information.
XDAS_Int32 IAUDDEC_Status::bitRate |
Average bit rate, in bits per second.
XDAS_Int32 IAUDDEC_Status::sampleRate |
Sampling frequency, in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.
XDAS_Int32 IAUDDEC_Status::numChannels |
Number of Channels. See IAUDIO_ChannelId.
XDAS_Int32 IAUDDEC_Status::numLFEChannels |
Number of LFE (Low Frequency Effects) channels in the stream.
XDAS_Int32 IAUDDEC_Status::outputFormat |
The output PCM format. See IAUDIO_PcmFormat.
XDAS_Int32 IAUDDEC_Status::autoPosition |
Flag to indicate support for random position decoding, which means that a stream can be decoded from any point. 0 indicates this feature is not supported, 1 indicates this feature is supported.
XDAS_Int32 IAUDDEC_Status::fastFwdLen |
Recommended fast forward length in bytes in case of random position decoding.
XDAS_Int32 IAUDDEC_Status::frameLen |
Number of samples decoded per process() call.
XDAS_Int32 IAUDDEC_Status::outputBitsPerSample |
Number of bits per output sample. For example, if the value of the field is 16, there are 16 output bits per PCM sample.
XDM_AlgBufInfo IAUDDEC_Status::bufInfo |
Input and output buffer information. See XDM_AlgBufInfo.