![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines the creation time parameters for all IAUDDEC1 instance objects. More...
#include <iauddec1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | outputPCMWidth |
XDAS_Int32 | pcmFormat |
XDAS_Int32 | dataEndianness |
Defines the creation time parameters for all IAUDDEC1 instance objects.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int32 IAUDDEC1_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IAUDDEC1_Params::outputPCMWidth |
Number of bits per output PCM Sample.
XDAS_Int32 IAUDDEC1_Params::pcmFormat |
Output PCM Format Block/Interleaved.
@sa IAUDIO_PcmFormat
XDAS_Int32 IAUDDEC1_Params::dataEndianness |
Endianness of output data.
@sa XDM_DataFormat