![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines the input arguments for all IAUDDEC1 instance process function. More...
#include <iauddec1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numBytes |
XDAS_Int32 | desiredChannelMode |
XDAS_Int32 | lfeFlag |
Defines the input arguments for all IAUDDEC1 instance process function.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IAUDDEC1_Fxns::process()
XDAS_Int32 IAUDDEC1_InArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IAUDDEC1_InArgs::numBytes |
Size of input data in bytes, provided to the algorithm for decoding.
XDAS_Int32 IAUDDEC1_InArgs::desiredChannelMode |
Desired Channel Configuration.
@sa IAUDIO_ChannelMode
XDAS_Int32 IAUDDEC1_InArgs::lfeFlag |
Flag indicating whether LFE channel data is desired in the output.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.