![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
This structure defines the codec parameters that can be modified after creation via control() calls. More...
#include <iauddec1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | downSampleSbrFlag |
This structure defines the codec parameters that can be modified after creation via control() calls.
@remarks It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error. @remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IAUDDEC1_Fxns::control()
XDAS_Int32 IAUDDEC1_DynamicParams::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IAUDDEC1_DynamicParams::downSampleSbrFlag |
Flag to indicate downsampling for SBR.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.