Codec Engine Application Programming Interface (API)
ce-w08
|
This header defines all types, constants, and functions shared by all implementations of the speech encoder algorithms.
Go to the source code of this file.
Data Structures | |
struct | ISPHENC1_Obj |
This must be the first field of all ISPHENC1 instance objects. More... | |
struct | ISPHENC1_Params |
Defines the creation time parameters for all ISPHENC1 instance objects. More... | |
struct | ISPHENC1_DynamicParams |
This structure defines the codec parameters that can be modified after creation via ISPHENC1_Fxns.control(). More... | |
struct | ISPHENC1_InArgs |
Defines the input arguments for all ISPHENC1 instance process function. More... | |
struct | ISPHENC1_Status |
Defines instance status parameters. More... | |
struct | ISPHENC1_OutArgs |
Defines the run time output arguments for all ISPHENC1 instance objects. More... | |
struct | ISPHENC1_Fxns |
Defines all of the operations on ISPHENC1 objects. More... |
Macros | |
#define | ISPHENC1_EOK XDM_EOK |
| |
#define | ISPHENC1_EFAIL XDM_EFAIL |
| |
#define | ISPHENC1_EUNSUPPORTED XDM_EUNSUPPORTED |
| |
#define | ISPHENC1_ENOOUTPUT 1 |
This value signifies no output being available at encoder, for example in the case of intermediate calls in 10msec frame size execution. |
Typedefs | |
typedef struct ISPHENC1_Obj | ISPHENC1_Obj |
This must be the first field of all ISPHENC1 instance objects. | |
typedef struct ISPHENC1_Obj * | ISPHENC1_Handle |
Opaque handle to an ISPHENC1 objects. | |
typedef struct ISPHENC1_Params | ISPHENC1_Params |
Defines the creation time parameters for all ISPHENC1 instance objects. | |
typedef struct ISPHENC1_DynamicParams | ISPHENC1_DynamicParams |
This structure defines the codec parameters that can be modified after creation via ISPHENC1_Fxns.control(). | |
typedef struct ISPHENC1_InArgs | ISPHENC1_InArgs |
Defines the input arguments for all ISPHENC1 instance process function. | |
typedef struct ISPHENC1_Status | ISPHENC1_Status |
Defines instance status parameters. | |
typedef struct ISPHENC1_OutArgs | ISPHENC1_OutArgs |
Defines the run time output arguments for all ISPHENC1 instance objects. | |
typedef IALG_Cmd | ISPHENC1_Cmd |
Defines the control commands for the ISPHENC1 module. | |
typedef struct ISPHENC1_Fxns | ISPHENC1_Fxns |
Defines all of the operations on ISPHENC1 objects. |
Enumerations | |
enum | ISPHENC1_FrameType { ISPHENC1_FTYPE_SPEECH = 0, ISPHENC1_FTYPE_SIDFRAME = 1, ISPHENC1_FTYPE_NODATA = 2 } |
Encoder frame types. More... |