![]() |
![]() |
Engine_AlgInfo | Properties of an Engine algorithm |
Engine_AlgInfo2 | Properties of an Engine algorithm. This structure is identical to Engine_AlgInfo except that the typeTab array of strings is replaced by a singie string called types . The string, types , represents a ';' separated list of inheritance hierarchies of the algorithm, for example, "ti.sdo.ce.video.IVIDDEC;ti.sdo.ce.test.xvideo.IVIDE" |
Engine_Attrs | Attributes of an Engine |
IALG_Fxns | Defines the fields and methods that must be supplied by all XDAIS algorithms |
IALG_MemRec | Memory records |
IALG_Obj | Algorithm instance object definition |
IALG_Params | Algorithm instance creation parameters |
IALG_Status | Pointer to algorithm specific status structure |
Memory_AllocParams | Parameters for Memory_alloc() & Memory_free() |
SKEL_Fxns | Table of functions defining the interface of a skeleton |
VISA_MsgHeader | VISA message header |