Uses the iceCrusher Benchmark counters.
enum TimestampProvider_CountType |
![](../../../../../Arrow_up.png) |
CountType
typedef enum TimestampProvider_CountType {
TimestampProvider_CountType_CYCLES,
// count cycles
TimestampProvider_CountType_INSTRUCTIONS
// count instructions
} TimestampProvider_CountType;
VALUES
CountType_CYCLES
Timestamp is in cycles.
CountType_INSTRUCTIONS
Timestamp is in instructions.
struct TimestampProvider_IceCrusherRegs |
![](../../../../../Arrow_up.png) |
typedef struct TimestampProvider_IceCrusherRegs {
UInt32 VER;
// 0x00 Revision
UInt32 DBGCFG;
// 0x04 Debug Config
UInt32 DBGCNTL;
// 0x08 Debug Control & Status
UInt32 RES_0C;
// 0x0C Reserved
UInt32 TRIGCNTL;
// 0x10 Trigger Control
UInt32 RSTCNTL;
// 0x14 Reset Control
UInt32 THRDIDCLM;
// 0x18 Thread ID Claim
UInt32 THRDID;
// 0x1c Thread ID
UInt32 INTCNTL;
// 0x20 Interrupt Control
UInt32 ETMCNTL;
// 0x24 ETM Control
UInt32 ETMPID;
// 0x28 ETM Process ID
UInt32 TEST;
// 0x2C Test
UInt32 SWBRKCTL;
// 0x30 Software Breakpoint Control
UInt32 SWBRKVAL;
// 0x34 Software Breakpoint Value
UInt32 RES_38;
// 0x38 Reserved
UInt32 RES_3C;
// 0x3C Reserved
UInt32 BCNT0CTRL;
// 0x40 Benchmark Counter 0 Control
UInt32 BCNT0;
// 0x44 Benchmark Counter 0
UInt32 RES_48;
// 0x48 Reserved
UInt32 RES_4C;
// 0x4C Reserved
UInt32 BCNT1CTRL;
// 0x50 Benchmark Counter 1 Control
UInt32 BCNT1;
// 0x54 Benchmark Counter 1
UInt32 RES_58[10];
// 0x58 - 0x7C Reserved
UInt32 HWBRK0CTL;
// 0x80 Hardware Breakpoint 0 Control
UInt32 HWBRK0ADR;
// 0x84 Hardware Breakpoint 0 Address
UInt32 HWBRK0ADRMASK;
// 0x88 Hardware Breakpoint 0 Address Mask
UInt32 RES_8C;
// 0x8C Reserved
UInt32 HWBRK1CTL;
// 0x90 Hardware Breakpoint 1 Control
UInt32 HWBRK1ADR;
// 0x94 Hardware Breakpoint 1 Address
UInt32 HWBRK1ADRMASK;
// 0x98 Hardware Breakpoint 1 Address Mask
UInt32 RES_9C;
// 0x9C Reserved
UInt32 HWBRK2CTL;
// 0xA0 Hardware Breakpoint 2 Control
UInt32 HWBRK2ADR;
// 0xA4 Hardware Breakpoint 2 Address
UInt32 HWBRK2ADRMASK;
// 0xA8 Hardware Breakpoint 2 Address Mask
UInt32 RES_AC;
// 0xAC Reserved
UInt32 HWBRK3CTL;
// 0xB0 Hardware Breakpoint 3 Control
UInt32 HWBRK3ADR;
// 0xB4 Hardware Breakpoint 3 Address
UInt32 HWBRK3ADRMASK;
// 0xB8 Hardware Breakpoint 3 Address Mask
UInt32 RES_BC[14];
// 0xBC - 0xF0 Reserved
UInt32 OS_LOCKSTS;
// 0xF4 OS Lock Status
UInt32 OS_LOCK;
// 0xF8 OS Lock
UInt32 DCON;
// 0xFC DCON Register
} TimestampProvider_IceCrusherRegs;
config TimestampProvider_A_counterInUse // module-wide |
![](../../../../../Arrow_up.png) |
Assert when configured benchmark counter is owned by CCS
extern const Assert_Id TimestampProvider_A_counterInUse;
config TimestampProvider_A_intControlInUse // module-wide |
![](../../../../../Arrow_up.png) |
Assert if interrupt control register is owned by CCS
extern const Assert_Id TimestampProvider_A_intControlInUse;
config TimestampProvider_benchmarkCounterId // module-wide |
![](../../../../../Arrow_up.png) |
ICECrusher Benchmark Counter id. 0 or 1. Default is 1
extern const UInt TimestampProvider_benchmarkCounterId;
config TimestampProvider_countType // module-wide |
![](../../../../../Arrow_up.png) |
Timestamp count type. Default is CYCLES.
CountType_INSTRUCTIONS only supported on benchmarkCounterId 1!!!
extern TimestampProvider_iceRegs |
![](../../../../../Arrow_up.png) |
TimestampProvider_get32() // module-wide |
![](../../../../../Arrow_up.png) |
Return a 32-bit timestamp
Bits32 TimestampProvider_get32();
RETURNS
Returns a 32-bit timestamp value.
Use
getFreq to convert this value into units of real time.
Returns a 32-bit timestamp value.
Use
getFreq to convert this value into units of real time.
SEE
TimestampProvider_get64() // module-wide |
![](../../../../../Arrow_up.png) |
Return a 64-bit timestamp
ARGUMENTS
result
pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit
wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the
hi field of
result is always set to 0; see
xdc.runtime.Types.Timestamp64. So, it is possible for
the
lo field to wrap around without any change to the
hi field.
Use
getFreq to convert this value into units of real
time.
pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit
wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the
hi field of
result is always set to 0; see
xdc.runtime.Types.Timestamp64. So, it is possible for
the
lo field to wrap around without any change to the
hi field.
Use
getFreq to convert this value into units of real
time.
SEE
TimestampProvider_getFreq() // module-wide |
![](../../../../../Arrow_up.png) |
Get the timestamp timer's frequency (in Hz)
ARGUMENTS
freq
pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit
wide frequency value where the timer's frequency (in Hz)
is written; see
xdc.runtime.Types.FreqHz.
This function provides a way of converting timestamp
values into units of real time.
pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit
wide frequency value where the timer's frequency (in Hz)
is written; see
xdc.runtime.Types.FreqHz.
This function provides a way of converting timestamp
values into units of real time.
SEE
Module-Wide Built-Ins |
![](../../../../../Arrow_up.png) |
// Get this module's unique id
Bool TimestampProvider_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool TimestampProvider_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 TimestampProvider_Module_getMask();
// Returns the diagnostics mask for this module
Void TimestampProvider_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
enum TimestampProvider.CountType |
![](../../../../../Arrow_up.png) |
CountType
XDCscript usage |
meta-domain |
values of type TimestampProvider.CountType
const TimestampProvider.CountType_CYCLES;
// count cycles
const TimestampProvider.CountType_INSTRUCTIONS;
// count instructions
VALUES
CountType_CYCLES
Timestamp is in cycles.
CountType_INSTRUCTIONS
Timestamp is in instructions.
C SYNOPSIS
struct TimestampProvider.IceCrusherRegs |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var obj = new TimestampProvider.IceCrusherRegs;
obj.VER = UInt32 ...
// 0x00 Revision
obj.DBGCFG = UInt32 ...
// 0x04 Debug Config
obj.DBGCNTL = UInt32 ...
// 0x08 Debug Control & Status
obj.RES_0C = UInt32 ...
// 0x0C Reserved
obj.TRIGCNTL = UInt32 ...
// 0x10 Trigger Control
obj.RSTCNTL = UInt32 ...
// 0x14 Reset Control
obj.THRDIDCLM = UInt32 ...
// 0x18 Thread ID Claim
obj.THRDID = UInt32 ...
// 0x1c Thread ID
obj.INTCNTL = UInt32 ...
// 0x20 Interrupt Control
obj.ETMCNTL = UInt32 ...
// 0x24 ETM Control
obj.ETMPID = UInt32 ...
// 0x28 ETM Process ID
obj.TEST = UInt32 ...
// 0x2C Test
obj.SWBRKCTL = UInt32 ...
// 0x30 Software Breakpoint Control
obj.SWBRKVAL = UInt32 ...
// 0x34 Software Breakpoint Value
obj.RES_38 = UInt32 ...
// 0x38 Reserved
obj.RES_3C = UInt32 ...
// 0x3C Reserved
obj.BCNT0CTRL = UInt32 ...
// 0x40 Benchmark Counter 0 Control
obj.BCNT0 = UInt32 ...
// 0x44 Benchmark Counter 0
obj.RES_48 = UInt32 ...
// 0x48 Reserved
obj.RES_4C = UInt32 ...
// 0x4C Reserved
obj.BCNT1CTRL = UInt32 ...
// 0x50 Benchmark Counter 1 Control
obj.BCNT1 = UInt32 ...
// 0x54 Benchmark Counter 1
obj.RES_58 = UInt32[10] ...
// 0x58 - 0x7C Reserved
obj.HWBRK0CTL = UInt32 ...
// 0x80 Hardware Breakpoint 0 Control
obj.HWBRK0ADR = UInt32 ...
// 0x84 Hardware Breakpoint 0 Address
obj.HWBRK0ADRMASK = UInt32 ...
// 0x88 Hardware Breakpoint 0 Address Mask
obj.RES_8C = UInt32 ...
// 0x8C Reserved
obj.HWBRK1CTL = UInt32 ...
// 0x90 Hardware Breakpoint 1 Control
obj.HWBRK1ADR = UInt32 ...
// 0x94 Hardware Breakpoint 1 Address
obj.HWBRK1ADRMASK = UInt32 ...
// 0x98 Hardware Breakpoint 1 Address Mask
obj.RES_9C = UInt32 ...
// 0x9C Reserved
obj.HWBRK2CTL = UInt32 ...
// 0xA0 Hardware Breakpoint 2 Control
obj.HWBRK2ADR = UInt32 ...
// 0xA4 Hardware Breakpoint 2 Address
obj.HWBRK2ADRMASK = UInt32 ...
// 0xA8 Hardware Breakpoint 2 Address Mask
obj.RES_AC = UInt32 ...
// 0xAC Reserved
obj.HWBRK3CTL = UInt32 ...
// 0xB0 Hardware Breakpoint 3 Control
obj.HWBRK3ADR = UInt32 ...
// 0xB4 Hardware Breakpoint 3 Address
obj.HWBRK3ADRMASK = UInt32 ...
// 0xB8 Hardware Breakpoint 3 Address Mask
obj.RES_BC = UInt32[14] ...
// 0xBC - 0xF0 Reserved
obj.OS_LOCKSTS = UInt32 ...
// 0xF4 OS Lock Status
obj.OS_LOCK = UInt32 ...
// 0xF8 OS Lock
obj.DCON = UInt32 ...
// 0xFC DCON Register
C SYNOPSIS
config TimestampProvider.A_counterInUse // module-wide |
![](../../../../../Arrow_up.png) |
Assert when configured benchmark counter is owned by CCS
XDCscript usage |
meta-domain |
msg: "A_counterInUse: Benchmark counter already claimed."
};
C SYNOPSIS
config TimestampProvider.A_intControlInUse // module-wide |
![](../../../../../Arrow_up.png) |
Assert if interrupt control register is owned by CCS
XDCscript usage |
meta-domain |
msg: "A_intCOntrolInUse: iceCrusher Int Control Register already claimed."
};
C SYNOPSIS
config TimestampProvider.benchmarkCounterId // module-wide |
![](../../../../../Arrow_up.png) |
ICECrusher Benchmark Counter id. 0 or 1. Default is 1
XDCscript usage |
meta-domain |
TimestampProvider.benchmarkCounterId = UInt 1;
C SYNOPSIS
config TimestampProvider.countType // module-wide |
![](../../../../../Arrow_up.png) |
Timestamp count type. Default is CYCLES.
CountType_INSTRUCTIONS only supported on benchmarkCounterId 1!!!
XDCscript usage |
meta-domain |
C SYNOPSIS
metaonly config TimestampProvider.common$ // module-wide |
![](../../../../../Arrow_up.png) |
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.