Additional ARM device-specific APIs are also provided.
IRQ Interrupts are nestable and can invoke SYS/BIOS functions.
FIQ Interrupts are non-nestable and cannot invoke SYS/BIOS functions.
The IRQ dispatcher re-enables IRQ interrupts prior to invoking the
ISR function associated with an interrupt but uses the CP INTC's
Host Interrupt Nesting Level Register (HINLR) to suppress lower
priority interrupts while the interrupt is being serviced.
The default FIQ handler does not re-enable FIQ interrupts nor
use the HINLR. It simply calls the registered FIQ ISR and returns.
To statically configure a non-dispatched interrupt:
To dynamically configure a non-dispatched interrupt:
const Hwi_NUM_INTERRUPTS |
![](../../../../../Arrow_up.png) |
The DA830 ARM Interrupt Controller has 101 defined interrupts
#define Hwi_NUM_INTERRUPTS (Int)101
enum Hwi_MaskingOption |
![](../../../../../Arrow_up.png) |
Shorthand interrupt masking options
typedef enum Hwi_MaskingOption {
Hwi_MaskingOption_NONE,
Hwi_MaskingOption_ALL,
Hwi_MaskingOption_SELF,
Hwi_MaskingOption_BITMASK,
Hwi_MaskingOption_LOWER
} Hwi_MaskingOption;
VALUES
MaskingOption_NONE
No interrupts are disabled
MaskingOption_ALL
All interrupts are disabled
MaskingOption_SELF
Only this interrupt is disabled
MaskingOption_BITMASK
User supplies interrupt enable masks
MaskingOption_LOWER
All current and lower priority
interrupts are disabled.
Only a few targets/devices truly
support this masking option. For those
that don't, this setting is treated
the same as MaskingOption_SELF.
typedef Hwi_FuncPtr |
![](../../../../../Arrow_up.png) |
Hwi create function type definition
typedef Void (*Hwi_FuncPtr)(UArg);
typedef Hwi_Irp |
![](../../../../../Arrow_up.png) |
Interrupt Return Pointer
DETAILS
This is the address of the interrupted instruction.
typedef Hwi_VectorFuncPtr |
![](../../../../../Arrow_up.png) |
Hwi vector function type definition
typedef Void (*Hwi_VectorFuncPtr)(Void);
struct Hwi_CPINTC |
![](../../../../../Arrow_up.png) |
Common Platform Interrupt Controller
typedef struct Hwi_CPINTC {
UInt32 REV;
// 0x00 Revision Register
UInt32 CR;
// 0x04 Control Register
UInt32 RES_08;
// 0x08 reserved
UInt32 HCR;
// 0x0C Host Control Register
UInt32 GER;
// 0x10 Global Enable Register
UInt32 RES_14;
// 0x14 reserved
UInt32 RES_18;
// 0x18 reserved
UInt32 GNLR;
// 0x1C Global Nesting Level Register
UInt32 SISR;
// 0x20 Status Index Set Register
UInt32 SICR;
// 0x24 Status Index Clear Register
UInt32 EISR;
// 0x28 Enable Index Set Register
UInt32 EICR;
// 0x2C Enable Index Clear Register
UInt32 GWER;
// 0x30 Global Wakeup Enable Register
UInt32 HIEISR;
// 0x34 Host Int Enable Index Set Register
UInt32 HIDISR;
// 0x38 Host Int Disable Index Set Register
UInt32 RES_3C;
// 0x3C reserved
UInt32 PPR;
// 0x40 Pacer Prescale Register
UInt32 RES_44;
// 0x44 reserved
UInt32 RES_48;
// 0x48 reserved
UInt32 RES_4C;
// 0x4C reserved
Ptr *VBR;
// 0x50 Vector Base Register
UInt32 VSR;
// 0x54 Vector Size Register
Ptr VNR;
// 0x58 Vector Null Register
UInt32 RES_5C[9];
// 0x5C-0x7C reserved
Int32 GPIR;
// 0x80 Global Prioritized Index Register
Ptr *GPVR;
// 0x84 Global Prioritized Vector Register
UInt32 RES_88;
// 0x88 reserved
UInt32 RES_8C;
// 0x8C reserved
UInt32 GSIER;
// 0x90 Global Secure Interrupt Enable Register
UInt32 SPIR;
// 0x94 Secure Prioritized Index Register
UInt32 RES_98[26];
// 0x98-0xFC reserved
UInt32 PPMR[64];
// 0x100-0x1FC Pacer Parameter/Map Registers
UInt32 SRSR[32];
// 0x200-0x27C Status Raw/Set Registers
UInt32 SECR[32];
// 0x280-0x2FC Status Enabled/Clear Registers
UInt32 ESR[32];
// 0x300-0x37C Enable Set Registers
UInt32 ECR[32];
// 0x380-0x3FC Enable Clear Registers
UInt8 CMR[1024];
// 0x400-0x7FC Channel Map Registers
UInt8 HIMR[256];
// 0x800-0x8FC Host Interrupt Map Registers
UInt32 HIPIR[256];
// 0x900-0xCFC Host Interrupt Pri Index Registers
UInt32 PR[32];
// 0xD00-0xD7C Polarity Registers
UInt32 TR[32];
// 0xD80-0xDFC Type Registers
UInt32 WER[64];
// 0xE00-0xEFC Wakeup Enable Registers
UInt32 DSR[64];
// 0xF00-0xFFC Debug Select Registers
UInt32 SER[32];
// 0x1000-0x107C Secure Enable Registers
UInt32 SDR[32];
// 0x1080-0x10FC Secure Disable Registers
UInt32 HINLR[256];
// 0x1100-0x14FC Host Interrupt Nesting Level Registers
UInt32 HIER[8];
// 0x1500-0x151F Host Interrupt Enable Registers
UInt32 RES_1520[56];
// 0x1520-0x15fC Reserved
Ptr *HIPVR[256];
// 0x1600-0x19fC Host Interrupt Prioritized Vector
} Hwi_CPINTC;
struct Hwi_HookSet |
![](../../../../../Arrow_up.png) |
Hwi hook set type definition
typedef struct Hwi_HookSet {
Void (*registerFxn)(Int);
} Hwi_HookSet;
DETAILS
The functions that make up a hookSet have certain restrictions. They
cannot call any Hwi instance functions other than Hwi_getHookContext()
and Hwi_setHookContext(). For all practical purposes, they should treat
the Hwi_Handle passed to these functions as an opaque handle.
struct Hwi_StackInfo |
![](../../../../../Arrow_up.png) |
Structure contains Hwi stack usage info
typedef struct Hwi_StackInfo {
SizeT hwiStackPeak;
SizeT hwiStackSize;
Ptr hwiStackBase;
} Hwi_StackInfo;
DETAILS
Used by getStackInfo() and viewGetStackInfo() functions
config Hwi_A_unsupportedMaskingOption // module-wide |
![](../../../../../Arrow_up.png) |
Assert when bad maskSetting parameter provided
extern const Assert_Id Hwi_A_unsupportedMaskingOption;
config Hwi_E_alreadyDefined // module-wide |
![](../../../../../Arrow_up.png) |
Error raised when Hwi is already defined
extern const Error_Id Hwi_E_alreadyDefined;
config Hwi_LD_end // module-wide |
![](../../../../../Arrow_up.png) |
Issued just after return from Hwi function (with interrupts disabled)
config Hwi_LM_begin // module-wide |
![](../../../../../Arrow_up.png) |
Issued just prior to Hwi function invocation (with interrupts disabled)
config Hwi_dispatcherAutoNestingSupport // module-wide |
![](../../../../../Arrow_up.png) |
Include interrupt nesting logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherAutoNestingSupport;
DETAILS
Default is true.
This option provides the user with the ability to optimize
interrupt dispatcher performance when support for interrupt
nesting is not required.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that manipulates interrupt mask
registers and enables and disables interrupts before and
after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts
enabled during the execution of your Hwi functions.
config Hwi_dispatcherIrpTrackingSupport // module-wide |
![](../../../../../Arrow_up.png) |
Controls whether the
dispatcher retains the interrupted thread's return address
extern const Bool Hwi_dispatcherIrpTrackingSupport;
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that keeps track of the interrupt's
return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return
address using the
getIrp API.
config Hwi_dispatcherSwiSupport // module-wide |
![](../../../../../Arrow_up.png) |
Include Swi scheduling logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherSwiSupport;
DETAILS
Default is inherited from
BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that Swis
will not be posted from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Swi scheduler
prior to returning from an interrupt.
config Hwi_dispatcherTaskSupport // module-wide |
![](../../../../../Arrow_up.png) |
Include Task scheduling logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherTaskSupport;
DETAILS
Default is inherited from
BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that no
Task scheduling APIs (ie
Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Task scheduler
prior to returning from an interrupt.
config Hwi_fiqStack // module-wide |
![](../../../../../Arrow_up.png) |
FIQ stack pointer. Default = null.
(Indicates that stack is to be created using
staticPlace()
extern const Ptr Hwi_fiqStack;
config Hwi_irqStack // module-wide |
![](../../../../../Arrow_up.png) |
IRQ stack pointer. Default = null.
(Indicates that stack is to be created using
staticPlace()
extern const Ptr Hwi_irqStack;
extern Hwi_cpIntc |
![](../../../../../Arrow_up.png) |
Physical Common Platform Interrupt Controller Device.
Short name is "Hwi_cpIntc"
Long name is "ti_sysbios_family_arm_da830_Hwi_cpIntc"
Hwi_CPINTC Hwi_cpIntc; // linked as extern ti_sysbios_family_arm_da830_Hwi_cpIntc
Hwi_beginFIQ() // module-wide |
![](../../../../../Arrow_up.png) |
Function to be invoked at the beginning of a
non-dispatched FIQ handler. Services cpIntc
Hwi_beginIRQ() // module-wide |
![](../../../../../Arrow_up.png) |
Function to be invoked at the beginning of a
non-dispatched IRQ handler. Services cpIntc
Hwi_clearInterrupt() // module-wide |
![](../../../../../Arrow_up.png) |
Clear a specific interrupt
Void Hwi_clearInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to clear
DETAILS
Clears a specific interrupt's pending status.
The implementation is family-specific.
Hwi_disable() // module-wide |
![](../../../../../Arrow_up.png) |
Globally disable interrupts
macro UInt Hwi_disable();
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_disable globally disables hardware interrupts and returns an
opaque key indicating whether interrupts were globally enabled or
disabled on entry to Hwi_disable().
The actual value of the key is target/device specific and is meant
to be passed to Hwi_restore().
Call Hwi_disable before a portion of a function that needs
to run without interruption. When critical processing is complete, call
Hwi_restore or Hwi_enable to reenable hardware interrupts.
Servicing of interrupts that occur while interrupts are disabled is
postponed until interrupts are reenabled. However, if the same type
of interrupt occurs several times while interrupts are disabled,
the interrupt's function is executed only once when interrupts are
reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if
an enabled interrupt occurred while interrupts are disabled.
Hwi_disable may be called from main(). However, since Hwi interrupts
are already disabled in main(), such a call has no effect.
CONSTRAINTS
If a Task switching API such as
Semaphore_pend(),
Semaphore_post(),
Task_sleep(), or
Task_yield()
is invoked which results in a context switch while
interrupts are disabled, an embedded call to
Hwi_enable occurs
on the way to the new thread context which unconditionally re-enables
interrupts. Interrupts will remain enabled until a subsequent
Hwi_disable
invocation.
Swis always run with interrupts enabled.
See
Swi_post() for a discussion Swis and
interrupts.
Hwi_disableFIQ() // module-wide |
![](../../../../../Arrow_up.png) |
Disable FIQ interrupts
RETURNS
previous FIQ interrupt enable/disable state
Hwi_disableIRQ() // module-wide |
![](../../../../../Arrow_up.png) |
Disable IRQ interrupts
RETURNS
previous IRQ interrupt enable/disable state
Hwi_disableInterrupt() // module-wide |
![](../../../../../Arrow_up.png) |
Disable a specific interrupt
UInt Hwi_disableInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to disable
RETURNS
key to restore previous enable/disable state
DETAILS
Disable a specific interrupt identified by an interrupt number.
Hwi_enable() // module-wide |
![](../../../../../Arrow_up.png) |
Globally enable interrupts
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_enable globally enables hardware interrupts and returns an
opaque key indicating whether interrupts were globally enabled or
disabled on entry to Hwi_enable().
The actual value of the key is target/device specific and is meant
to be passed to Hwi_restore().
This function is
called as part of SYS/BIOS Startup_POST_APP_MAIN phase.
Hardware interrupts are enabled unless a call to Hwi_disable disables
them.
Servicing of interrupts that occur while interrupts are disabled is
postponed until interrupts are reenabled. However, if the same type
of interrupt occurs several times while interrupts are disabled,
the interrupt's function is executed only once when interrupts are
reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if
an enabled interrupt occurred while interrupts are disabled.
Any call to Hwi_enable enables interrupts, even if Hwi_disable has
been called several times.
Hwi_enable must not be called from main().
Hwi_enableFIQ() // module-wide |
![](../../../../../Arrow_up.png) |
Enable FIQ interrupts
RETURNS
previous FIQ interrupt enable/disable state
Hwi_enableIRQ() // module-wide |
![](../../../../../Arrow_up.png) |
Enable IRQ interrupts
ARGUMENTS
key
enable/disable state to restore
Hwi_enableInterrupt() // module-wide |
![](../../../../../Arrow_up.png) |
Enable a specific interrupt
UInt Hwi_enableInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to enable
RETURNS
key to restore previous enable/disable state
DETAILS
Enables a specific interrupt identified by an interrupt number.
Hwi_endFIQ() // module-wide |
![](../../../../../Arrow_up.png) |
Function to be invoked at the end of a
non-dispatched FIQ handler. Services cpIntc
Hwi_endIRQ() // module-wide |
![](../../../../../Arrow_up.png) |
Function to be invoked at the end of a
non-dispatched IRQ handler. Services cpIntc
Hwi_getHandle() // module-wide |
![](../../../../../Arrow_up.png) |
Returns Hwi_handle associated with intNum
ARGUMENTS
intNum
interrupt number
Hwi_getStackInfo() // module-wide |
![](../../../../../Arrow_up.png) |
Get Hwi stack usage Info
Bool Hwi_getStackInfo(
IHwi_StackInfo *
stkInfo,
Bool computeStackDepth);
ARGUMENTS
stkInfo
pointer to structure of type StackInfo
computeStackDepth
decides whether to compute stack depth
RETURNS
boolean to indicate a stack overflow
DETAILS
getStackInfo returns the Hwi stack usage info to its calling
function by filling stack base address, stack size and stack
peak fields in the
StackInfo structure.
getStackInfo accepts two arguments, a pointer to a structure
of type
StackInfo and a boolean. If the boolean is set
to true, the function computes the stack depth and fills the
stack peak field in the StackInfo structure. If a stack overflow
is detected, the stack depth is not computed. If the boolean is
set to false, the function only checks for a stack overflow.
The isr stack is always checked for an overflow and a boolean
is returned to indicate whether an overflow occured.
Below is an example of calling getStackInfo() API:
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/hal/Hwi.h>
#include <ti/sysbios/knl/Swi.h>
#include <ti/sysbios/knl/Task.h>
Swi_Handle swi0;
volatile Bool swiStackOverflow = FALSE;
Void swi0Fxn(UArg arg1, UArg arg2)
{
Hwi_StackInfo stkInfo;
// Request stack depth
swiStackOverflow = Hwi_getStackInfo(&stkInfo, TRUE);
// Alternately, we can omit the request for stack depth and
// request only the stack base and stack size (the check for
// stack overflow is always performed):
//
// swiStackOverflow = Hwi_getStackInfo(&stkInfo, FALSE);
if (swiStackOverflow) {
// isr Stack Overflow detected
}
}
Void idleTask()
{
Swi_post(swi0);
}
Int main(Int argc, char* argv[])
{
swi0 = Swi_create(swi0Fxn, NULL, NULL);
BIOS_start();
return (0);
}
Hwi_post() // module-wide |
![](../../../../../Arrow_up.png) |
Generate an interrupt for test purposes
Void Hwi_post(UInt intNum);
ARGUMENTS
intNum
ID of interrupt to generate
Hwi_restore() // module-wide |
![](../../../../../Arrow_up.png) |
Globally restore interrupts
macro Void Hwi_restore(UInt key);
ARGUMENTS
key
enable/disable state to restore
DETAILS
Hwi_restore globally restores interrupts to the state determined
by the key argument provided by a previous invocation of Hwi_disable.
A context switch may occur when calling Hwi_restore if Hwi_restore
reenables interrupts and another Hwi occurred while interrupts were
disabled.
Hwi_restore may be called from main(). However, since Hwi_enable
cannot be called from main(), interrupts are always disabled in
main(), and a call to Hwi_restore has no effect.
Hwi_restoreFIQ() // module-wide |
![](../../../../../Arrow_up.png) |
Restore FIQ interrupts
Void Hwi_restoreFIQ(UInt key);
ARGUMENTS
key
enable/disable state to restore
Hwi_restoreIRQ() // module-wide |
![](../../../../../Arrow_up.png) |
Restore IRQ interrupts
Void Hwi_restoreIRQ(UInt key);
ARGUMENTS
key
enable/disable state to restore
Hwi_restoreInterrupt() // module-wide |
![](../../../../../Arrow_up.png) |
Restore a specific interrupt's enabled/disabled state
Void Hwi_restoreInterrupt(UInt intNum, UInt key);
ARGUMENTS
intNum
interrupt number to restore
key
key returned from enableInt or disableInt
DETAILS
Restores a specific interrupt identified by an interrupt number.
restoreInterrupt is generally used to restore an interrupt to its state
before
disableInterrupt or
enableInterrupt was
invoked
Hwi_setPriority() // module-wide |
![](../../../../../Arrow_up.png) |
Set an interrupt's relative priority
Void Hwi_setPriority(UInt intNum, UInt priority);
ARGUMENTS
intNum
ID of interrupt
priority
priority
DETAILS
Valid priorities are 0 - 31. 0 is highest priority.
Priorities 0 - 1 are routed to the ARM's FIQ interrupt.
Priorities 2 - 31 are routed to the ARM's IRQ interrupt.
Hwi_startup() // module-wide |
![](../../../../../Arrow_up.png) |
Initially enable interrupts
DETAILS
Called within BIOS_start
Module-Wide Built-Ins |
![](../../../../../Arrow_up.png) |
// Get this module's unique id
Bool Hwi_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Hwi_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Hwi_Module_getMask();
// Returns the diagnostics mask for this module
Void Hwi_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
![](../../../../../Arrow_up.png) |
typedef struct Hwi_Object Hwi_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct Hwi_Struct Hwi_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
![](../../../../../Arrow_up.png) |
typedef struct Hwi_Params {
// Instance config-params structure
// Common per-instance configs
UArg arg;
// ISR function argument. Default is 0
Bool enableInt;
// Enable this interrupt when object is created? Default is true
Int eventId;
// Interrupt event ID (Interrupt Selection Number)
Int priority;
// Interrupt priority.
Valid priorities are 0 - 31. 0 is highest priority.
Priorities 0 - 1 are routed to the ARM's FIQ interrupt.
Priorities 2 - 31 are routed to the ARM's IRQ interrupt.
The default is 31 which is the lowest priority IRQ interrupt
} Hwi_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config Hwi_arg // instance |
![](../../../../../Arrow_up.png) |
ISR function argument. Default is 0
config Hwi_enableInt // instance |
![](../../../../../Arrow_up.png) |
Enable this interrupt when object is created? Default is true
config Hwi_eventId // instance |
![](../../../../../Arrow_up.png) |
Interrupt event ID (Interrupt Selection Number)
DETAILS
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored.
config Hwi_maskSetting // instance |
![](../../../../../Arrow_up.png) |
maskSetting. Default is Hwi_MaskingOption_SELF
config Hwi_priority // instance |
![](../../../../../Arrow_up.png) |
Interrupt priority.
Valid priorities are 0 - 31. 0 is highest priority.
Priorities 0 - 1 are routed to the ARM's FIQ interrupt.
Priorities 2 - 31 are routed to the ARM's IRQ interrupt.
The default is 31 which is the lowest priority IRQ interrupt
DETAILS
The default value of -1 is used as a flag to indicate
the lowest (logical) device-specific priority value.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored.
Instance Creation |
![](../../../../../Arrow_up.png) |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
intNum
interrupt number
hwiFxn
pointer to ISR function
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the
function specified by the fxn parameter and the attributes
specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a
default set of values. Otherwise, the following properties
are specified by a structure of type Hwi_Params.
- The arg element is a generic argument that is passed to the plugged
function as its only parameter. The default value is 0.
- The enableInt element determines whether the interrupt should be
enabled in the IER by create.
- The maskSetting element defines the dispatcherAutoNestingSupport
behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.
Instance Deletion |
![](../../../../../Arrow_up.png) |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
Hwi_getFunc() // instance |
![](../../../../../Arrow_up.png) |
Get Hwi function and arg
ARGUMENTS
handle
handle of a previously-created Hwi instance object
arg
pointer for returning hwi's ISR function argument
RETURNS
hwi's ISR function
Hwi_getHookContext() // instance |
![](../../../../../Arrow_up.png) |
Get hook instance's context for a Hwi
Ptr Hwi_getHookContext(
Hwi_Handle handle,
Int id);
ARGUMENTS
handle
handle of a previously-created Hwi instance object
RETURNS
hook instance's context for hwi
Hwi_getIrp() // instance |
![](../../../../../Arrow_up.png) |
Get address of interrupted instruction
ARGUMENTS
handle
handle of a previously-created Hwi instance object
RETURNS
most current IRP of a Hwi
Hwi_reconfig() // instance |
![](../../../../../Arrow_up.png) |
Reconfigure a dispatched interrupt
ARGUMENTS
handle
handle of a previously-created Hwi instance object
Hwi_setFunc() // instance |
![](../../../../../Arrow_up.png) |
Overwrite Hwi function and arg
ARGUMENTS
handle
handle of a previously-created Hwi instance object
fxn
pointer to ISR function
arg
argument to ISR function
DETAILS
Replaces a Hwi object's hwiFxn function originally
provided in
create.
Hwi_setHookContext() // instance |
![](../../../../../Arrow_up.png) |
Set hook instance's context for a Hwi
Void Hwi_setHookContext(
Hwi_Handle handle,
Int id,
Ptr hookContext);
ARGUMENTS
handle
handle of a previously-created Hwi instance object
id
hook instance's ID
hookContext
value to write to context
Instance Convertors |
![](../../../../../Arrow_up.png) |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
![](../../../../../Arrow_up.png) |
Int Hwi_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
const Hwi.NUM_INTERRUPTS |
![](../../../../../Arrow_up.png) |
The DA830 ARM Interrupt Controller has 101 defined interrupts
XDCscript usage |
meta-domain |
const Hwi.NUM_INTERRUPTS = 101;
C SYNOPSIS
enum Hwi.MaskingOption |
![](../../../../../Arrow_up.png) |
Shorthand interrupt masking options
XDCscript usage |
meta-domain |
values of type Hwi.MaskingOption
const Hwi.MaskingOption_NONE;
const Hwi.MaskingOption_ALL;
const Hwi.MaskingOption_SELF;
const Hwi.MaskingOption_BITMASK;
const Hwi.MaskingOption_LOWER;
VALUES
MaskingOption_NONE
No interrupts are disabled
MaskingOption_ALL
All interrupts are disabled
MaskingOption_SELF
Only this interrupt is disabled
MaskingOption_BITMASK
User supplies interrupt enable masks
MaskingOption_LOWER
All current and lower priority
interrupts are disabled.
Only a few targets/devices truly
support this masking option. For those
that don't, this setting is treated
the same as MaskingOption_SELF.
C SYNOPSIS
struct Hwi.CPINTC |
![](../../../../../Arrow_up.png) |
Common Platform Interrupt Controller
XDCscript usage |
meta-domain |
var obj = new Hwi.CPINTC;
obj.REV = UInt32 ...
// 0x00 Revision Register
obj.CR = UInt32 ...
// 0x04 Control Register
obj.RES_08 = UInt32 ...
// 0x08 reserved
obj.HCR = UInt32 ...
// 0x0C Host Control Register
obj.GER = UInt32 ...
// 0x10 Global Enable Register
obj.RES_14 = UInt32 ...
// 0x14 reserved
obj.RES_18 = UInt32 ...
// 0x18 reserved
obj.GNLR = UInt32 ...
// 0x1C Global Nesting Level Register
obj.SISR = UInt32 ...
// 0x20 Status Index Set Register
obj.SICR = UInt32 ...
// 0x24 Status Index Clear Register
obj.EISR = UInt32 ...
// 0x28 Enable Index Set Register
obj.EICR = UInt32 ...
// 0x2C Enable Index Clear Register
obj.GWER = UInt32 ...
// 0x30 Global Wakeup Enable Register
obj.HIEISR = UInt32 ...
// 0x34 Host Int Enable Index Set Register
obj.HIDISR = UInt32 ...
// 0x38 Host Int Disable Index Set Register
obj.RES_3C = UInt32 ...
// 0x3C reserved
obj.PPR = UInt32 ...
// 0x40 Pacer Prescale Register
obj.RES_44 = UInt32 ...
// 0x44 reserved
obj.RES_48 = UInt32 ...
// 0x48 reserved
obj.RES_4C = UInt32 ...
// 0x4C reserved
obj.VBR = Ptr* ...
// 0x50 Vector Base Register
obj.VSR = UInt32 ...
// 0x54 Vector Size Register
obj.VNR = Ptr ...
// 0x58 Vector Null Register
obj.RES_5C = UInt32[9] ...
// 0x5C-0x7C reserved
obj.GPIR = Int32 ...
// 0x80 Global Prioritized Index Register
obj.GPVR = Ptr* ...
// 0x84 Global Prioritized Vector Register
obj.RES_88 = UInt32 ...
// 0x88 reserved
obj.RES_8C = UInt32 ...
// 0x8C reserved
obj.GSIER = UInt32 ...
// 0x90 Global Secure Interrupt Enable Register
obj.SPIR = UInt32 ...
// 0x94 Secure Prioritized Index Register
obj.RES_98 = UInt32[26] ...
// 0x98-0xFC reserved
obj.PPMR = UInt32[64] ...
// 0x100-0x1FC Pacer Parameter/Map Registers
obj.SRSR = UInt32[32] ...
// 0x200-0x27C Status Raw/Set Registers
obj.SECR = UInt32[32] ...
// 0x280-0x2FC Status Enabled/Clear Registers
obj.ESR = UInt32[32] ...
// 0x300-0x37C Enable Set Registers
obj.ECR = UInt32[32] ...
// 0x380-0x3FC Enable Clear Registers
obj.CMR = UInt8[1024] ...
// 0x400-0x7FC Channel Map Registers
obj.HIMR = UInt8[256] ...
// 0x800-0x8FC Host Interrupt Map Registers
obj.HIPIR = UInt32[256] ...
// 0x900-0xCFC Host Interrupt Pri Index Registers
obj.PR = UInt32[32] ...
// 0xD00-0xD7C Polarity Registers
obj.TR = UInt32[32] ...
// 0xD80-0xDFC Type Registers
obj.WER = UInt32[64] ...
// 0xE00-0xEFC Wakeup Enable Registers
obj.DSR = UInt32[64] ...
// 0xF00-0xFFC Debug Select Registers
obj.SER = UInt32[32] ...
// 0x1000-0x107C Secure Enable Registers
obj.SDR = UInt32[32] ...
// 0x1080-0x10FC Secure Disable Registers
obj.HINLR = UInt32[256] ...
// 0x1100-0x14FC Host Interrupt Nesting Level Registers
obj.HIER = UInt32[8] ...
// 0x1500-0x151F Host Interrupt Enable Registers
obj.RES_1520 = UInt32[56] ...
// 0x1520-0x15fC Reserved
obj.HIPVR = Ptr*[256] ...
// 0x1600-0x19fC Host Interrupt Prioritized Vector
C SYNOPSIS
struct Hwi.HookSet |
![](../../../../../Arrow_up.png) |
Hwi hook set type definition
XDCscript usage |
meta-domain |
var obj = new Hwi.HookSet;
obj.registerFxn = Void(*)(Int) ...
DETAILS
The functions that make up a hookSet have certain restrictions. They
cannot call any Hwi instance functions other than Hwi_getHookContext()
and Hwi_setHookContext(). For all practical purposes, they should treat
the Hwi_Handle passed to these functions as an opaque handle.
C SYNOPSIS
metaonly struct Hwi.NonDispatchedInterrupt |
![](../../../../../Arrow_up.png) |
non-dispatched interrupt object.
provided so that XGCONF users can easily plug non-dispatched interrupts
XDCscript usage |
meta-domain |
var obj = new Hwi.NonDispatchedInterrupt;
obj.intNum = Int ...
obj.fxn = Void(*)(Void) ...
// "Hwi_plug'd" ISR function
obj.priority = UInt ...
obj.enableInt = Bool ...
struct Hwi.StackInfo |
![](../../../../../Arrow_up.png) |
Structure contains Hwi stack usage info
XDCscript usage |
meta-domain |
var obj = new Hwi.StackInfo;
obj.hwiStackPeak = SizeT ...
obj.hwiStackSize = SizeT ...
obj.hwiStackBase = Ptr ...
DETAILS
Used by getStackInfo() and viewGetStackInfo() functions
C SYNOPSIS
config Hwi.A_unsupportedMaskingOption // module-wide |
![](../../../../../Arrow_up.png) |
Assert when bad maskSetting parameter provided
XDCscript usage |
meta-domain |
msg: "A_unsupportedMaskingOption: unsupported maskSetting."
};
C SYNOPSIS
config Hwi.E_alreadyDefined // module-wide |
![](../../../../../Arrow_up.png) |
Error raised when Hwi is already defined
XDCscript usage |
meta-domain |
msg: "E_alreadyDefined: Hwi already defined: intr# %d"
};
C SYNOPSIS
config Hwi.LD_end // module-wide |
![](../../../../../Arrow_up.png) |
Issued just after return from Hwi function (with interrupts disabled)
XDCscript usage |
meta-domain |
msg: "LD_end: hwi: 0x%x"
};
C SYNOPSIS
config Hwi.LM_begin // module-wide |
![](../../../../../Arrow_up.png) |
Issued just prior to Hwi function invocation (with interrupts disabled)
XDCscript usage |
meta-domain |
msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
};
C SYNOPSIS
config Hwi.dispatcherAutoNestingSupport // module-wide |
![](../../../../../Arrow_up.png) |
Include interrupt nesting logic in interrupt dispatcher?
XDCscript usage |
meta-domain |
Hwi.dispatcherAutoNestingSupport = Bool true;
DETAILS
Default is true.
This option provides the user with the ability to optimize
interrupt dispatcher performance when support for interrupt
nesting is not required.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that manipulates interrupt mask
registers and enables and disables interrupts before and
after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts
enabled during the execution of your Hwi functions.
C SYNOPSIS
config Hwi.dispatcherIrpTrackingSupport // module-wide |
![](../../../../../Arrow_up.png) |
Controls whether the
dispatcher retains the interrupted thread's return address
XDCscript usage |
meta-domain |
Hwi.dispatcherIrpTrackingSupport = Bool true;
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that keeps track of the interrupt's
return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return
address using the
getIrp API.
C SYNOPSIS
config Hwi.dispatcherSwiSupport // module-wide |
![](../../../../../Arrow_up.png) |
Include Swi scheduling logic in interrupt dispatcher?
XDCscript usage |
meta-domain |
Hwi.dispatcherSwiSupport = Bool undefined;
DETAILS
Default is inherited from
BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that Swis
will not be posted from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Swi scheduler
prior to returning from an interrupt.
C SYNOPSIS
config Hwi.dispatcherTaskSupport // module-wide |
![](../../../../../Arrow_up.png) |
Include Task scheduling logic in interrupt dispatcher?
XDCscript usage |
meta-domain |
Hwi.dispatcherTaskSupport = Bool undefined;
DETAILS
Default is inherited from
BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that no
Task scheduling APIs (ie
Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Task scheduler
prior to returning from an interrupt.
C SYNOPSIS
config Hwi.fiqStack // module-wide |
![](../../../../../Arrow_up.png) |
FIQ stack pointer. Default = null.
(Indicates that stack is to be created using
staticPlace()
XDCscript usage |
meta-domain |
C SYNOPSIS
config Hwi.irqStack // module-wide |
![](../../../../../Arrow_up.png) |
IRQ stack pointer. Default = null.
(Indicates that stack is to be created using
staticPlace()
XDCscript usage |
meta-domain |
C SYNOPSIS
metaonly config Hwi.common$ // module-wide |
![](../../../../../Arrow_up.png) |
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config Hwi.dataAbortFunc // module-wide |
![](../../../../../Arrow_up.png) |
Data abort exception handler. Default is self loop
XDCscript usage |
meta-domain |
Hwi.dataAbortFunc = Void(*)(Void) undefined;
metaonly config Hwi.fiqFunc // module-wide |
![](../../../../../Arrow_up.png) |
FIQ interrupt handler. Default is internal FIQ dispatcher
XDCscript usage |
meta-domain |
Hwi.fiqFunc = Void(*)(Void) undefined;
metaonly config Hwi.fiqStackSection // module-wide |
![](../../../../../Arrow_up.png) |
Memory section used for FIQ stack
Default is null
XDCscript usage |
meta-domain |
Hwi.fiqStackSection = String null;
metaonly config Hwi.fiqStackSize // module-wide |
![](../../../../../Arrow_up.png) |
FIQ stack size in bytes.
Default is 1024 bytes
XDCscript usage |
meta-domain |
Hwi.fiqStackSize = SizeT 1024;
metaonly config Hwi.irqFunc // module-wide |
![](../../../../../Arrow_up.png) |
IRQ interrupt handler. Default is internal IRQ dispatcher
XDCscript usage |
meta-domain |
Hwi.irqFunc = Void(*)(Void) undefined;
metaonly config Hwi.irqStackSection // module-wide |
![](../../../../../Arrow_up.png) |
Memory section used for IRQ stack
Default is null
XDCscript usage |
meta-domain |
Hwi.irqStackSection = String null;
metaonly config Hwi.irqStackSize // module-wide |
![](../../../../../Arrow_up.png) |
IRQ stack size in bytes.
Default is 256 bytes.
This is enough room for 32 nested IRQ interrupts
XDCscript usage |
meta-domain |
Hwi.irqStackSize = SizeT 256;
DETAILS
An IRQ interrupt pushes 2 32bit words onto the IRQ stack.
metaonly config Hwi.nonDispatchedInterrupts // module-wide |
![](../../../../../Arrow_up.png) |
non-dispatched interrupt array.
provided so that XGCONF users can easily plug non-dispatched interrupts
XDCscript usage |
meta-domain |
metaonly config Hwi.prefetchAbortFunc // module-wide |
![](../../../../../Arrow_up.png) |
Prefetch abort exception handler. Default is self loop
XDCscript usage |
meta-domain |
Hwi.prefetchAbortFunc = Void(*)(Void) undefined;
metaonly config Hwi.reservedFunc // module-wide |
![](../../../../../Arrow_up.png) |
Reserved exception handler. Default is self loop
XDCscript usage |
meta-domain |
Hwi.reservedFunc = Void(*)(Void) undefined;
metaonly config Hwi.resetFunc // module-wide |
![](../../../../../Arrow_up.png) |
Reset Handler. Default is c_int00
XDCscript usage |
meta-domain |
Hwi.resetFunc = Void(*)(Void) undefined;
metaonly config Hwi.swiFunc // module-wide |
![](../../../../../Arrow_up.png) |
SWI Handler. Default is internal SWI handler
XDCscript usage |
meta-domain |
Hwi.swiFunc = Void(*)(Void) undefined;
metaonly config Hwi.undefinedInstFunc // module-wide |
![](../../../../../Arrow_up.png) |
Undefined instruction exception handler. Default is self loop
XDCscript usage |
meta-domain |
Hwi.undefinedInstFunc = Void(*)(Void) undefined;
metaonly config Hwi.vectorTableAddress // module-wide |
![](../../../../../Arrow_up.png) |
Location of the Interrupt Vector Table
XDCscript usage |
meta-domain |
Hwi.vectorTableAddress = Ptr 0xffff0040;
DETAILS
The default placement of the Interrupt Vector Table
is immediately after the ARM exception table located
at 0xffff0000.
The vector table is internally assigned to the ".vectorTable"
memory section.
metaonly Hwi.addHookSet() // module-wide |
![](../../../../../Arrow_up.png) |
addHookSet is used in a config file to add a hook set (defined
by struct HookSet)
XDCscript usage |
meta-domain |
ARGUMENTS
hook
structure of type HookSet
DETAILS
HookSet structure elements may be omitted, in which case those
elements will not exist.
metaonly Hwi.plugMeta() // module-wide |
![](../../../../../Arrow_up.png) |
Statically plug an interrupt vector with an ISR address
XDCscript usage |
meta-domain |
Hwi.plugMeta(UInt intNum, Void(*)(Void) fxn) returns Void
ARGUMENTS
intNum
interrupt number
fxn
pointer to ISR function
Instance Config Parameters |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
// Instance config-params object
params.arg = UArg 0;
// ISR function argument. Default is 0
params.enableInt = Bool true;
// Enable this interrupt when object is created? Default is true
params.eventId = Int -1;
// Interrupt event ID (Interrupt Selection Number)
params.priority = Int 31;
// Interrupt priority.
Valid priorities are 0 - 31. 0 is highest priority.
Priorities 0 - 1 are routed to the ARM's FIQ interrupt.
Priorities 2 - 31 are routed to the ARM's IRQ interrupt.
The default is 31 which is the lowest priority IRQ interrupt
config Hwi.arg // instance |
![](../../../../../Arrow_up.png) |
ISR function argument. Default is 0
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.arg = UArg 0;
C SYNOPSIS
config Hwi.enableInt // instance |
![](../../../../../Arrow_up.png) |
Enable this interrupt when object is created? Default is true
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.enableInt = Bool true;
C SYNOPSIS
config Hwi.eventId // instance |
![](../../../../../Arrow_up.png) |
Interrupt event ID (Interrupt Selection Number)
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.eventId = Int -1;
DETAILS
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored.
C SYNOPSIS
config Hwi.maskSetting // instance |
![](../../../../../Arrow_up.png) |
maskSetting. Default is Hwi_MaskingOption_SELF
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
C SYNOPSIS
config Hwi.priority // instance |
![](../../../../../Arrow_up.png) |
Interrupt priority.
Valid priorities are 0 - 31. 0 is highest priority.
Priorities 0 - 1 are routed to the ARM's FIQ interrupt.
Priorities 2 - 31 are routed to the ARM's IRQ interrupt.
The default is 31 which is the lowest priority IRQ interrupt
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.priority = Int 31;
DETAILS
The default value of -1 is used as a flag to indicate
the lowest (logical) device-specific priority value.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored.
C SYNOPSIS
Instance Creation |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = Hwi.create(Int intNum, Void(*)(UArg) hwiFxn, params);
// Create an instance-object
ARGUMENTS
intNum
interrupt number
hwiFxn
pointer to ISR function
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the
function specified by the fxn parameter and the attributes
specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a
default set of values. Otherwise, the following properties
are specified by a structure of type Hwi_Params.
- The arg element is a generic argument that is passed to the plugged
function as its only parameter. The default value is 0.
- The enableInt element determines whether the interrupt should be
enabled in the IER by create.
- The maskSetting element defines the dispatcherAutoNestingSupport
behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.