Configuration example: The following XDC configuration statements
create a logger instance, plugs in the user defined functions, assign it as
the default logger for all modules, and enable
USER1 logging in all
all modules of the package
my.pkg. See the
Diags.setMaskMeta() function for details on
specifying the module names.
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var Diags = xdc.useModule('xdc.runtime.Diags');
var LoggerCallback = xdc.useModule('xdc.runtime.LoggerCallback');
LoggerCallback.outputFxn = "&userOutputFunc";
LoggerCallback.createInstFxn = "&userCreateInstFunc";
var loggerParams = new Logger.Params();
loggerParams.arg = 1;
Defaults.common$.logger = LoggerCallback.create(loggerParams);
Diags.setMaskMeta("my.pkg.%", Diags.USER1, Diags.RUNTIME_ON);
typedef LoggerCallback_CreateInstFxn |
![](../../Arrow_up.png) |
Logger instance create callback function signature
typedef UArg (*LoggerCallback_CreateInstFxn)(UArg);
DETAILS
LoggerCallback.arg is passed as an argument to this function.
The return value from this function will be passed as an argument
to the outputFxn
. In case of multiple LoggerCallback instances, the
return value can be used in outputFxn` to differentiate among the
instances.
typedef LoggerCallback_OutputFxn |
![](../../Arrow_up.png) |
Character output callback function signature
typedef Void (*
LoggerCallback_OutputFxn)(
UArg,
Log_EventRec*,
Int);
DETAILS
The first argument is the parameter returned by the call to
createInstFxn.
The second argument is a pointer to
Log.EventRec record.
The third argument is the number of arguments in
Log.EventRec
Note: Only evt and arg fields in Log_EventRec record are filled and
passed to the user supplied function.
config LoggerCallback_createInstFxn // module-wide |
![](../../Arrow_up.png) |
User supplied logger instance create function
DETAILS
This function is called when the
LoggerCallback.create is
called.
By default, this function is configured with a default create function.
The default create function returns 0 always.
config LoggerCallback_outputFxn // module-wide |
![](../../Arrow_up.png) |
User supplied character callback function
DETAILS
This function is called when the
Log module needs to output an event.
e.g.
Log.write4() or
Log.print2()
By default, this function is configured with a default output function.
The default function does nothing and returns.
Module-Wide Built-Ins |
![](../../Arrow_up.png) |
// Get this module's unique id
Bool LoggerCallback_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool LoggerCallback_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 LoggerCallback_Module_getMask();
// Returns the diagnostics mask for this module
Void LoggerCallback_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
![](../../Arrow_up.png) |
typedef struct LoggerCallback_Object LoggerCallback_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct LoggerCallback_Struct LoggerCallback_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
![](../../Arrow_up.png) |
typedef struct LoggerCallback_Params {
// Instance config-params structure
// Common per-instance configs
UArg arg;
// User supplied argument for the user supplied create function
} LoggerCallback_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config LoggerCallback_arg // instance |
![](../../Arrow_up.png) |
User supplied argument for the user supplied create function
DETAILS
This user supplied argument will be passed back as an argument to the
createInstFxn function. It can be used by the
LoggerCallback.createInstFxn function at runtime to
differentiate between the multiple logger instances configured in the
user config script.
The user can skip configuring this argument. In such a case, the
default value 0 will be passed back as an argument to the
createInstFxn function.
Instance Creation |
![](../../Arrow_up.png) |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
Instance Deletion |
![](../../Arrow_up.png) |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
LoggerCallback_disable() // instance |
![](../../Arrow_up.png) |
Disable a log
ARGUMENTS
handle
handle of a previously-created LoggerCallback instance object
DETAILS
Events written to a disabled log are silently discarded.
RETURNS
The function returns the state of the log (TRUE if enabled,
FALSE if disabled) before the call. This return value allows
clients to restore the previous state.
Note: not thread safe.
LoggerCallback_enable() // instance |
![](../../Arrow_up.png) |
Enable a log
ARGUMENTS
handle
handle of a previously-created LoggerCallback instance object
RETURNS
The function returns the state of the log (TRUE if enabled,
FALSE if disabled) before the call. This return value allows
clients to restore the previous state.
Note: not thread safe.
LoggerCallback_write0() // instance |
![](../../Arrow_up.png) |
Process a log event with 0 arguments
ARGUMENTS
handle
handle of a previously-created LoggerCallback instance object
DETAILS
Same as write4 except with 0 arguments rather than 4.
SEE
LoggerCallback_write1() // instance |
![](../../Arrow_up.png) |
Process a log event with 1 arguments
ARGUMENTS
handle
handle of a previously-created LoggerCallback instance object
DETAILS
Same as write4 except with 1 arguments rather than 4.
SEE
LoggerCallback_write2() // instance |
![](../../Arrow_up.png) |
Process a log event with 2 arguments
ARGUMENTS
handle
handle of a previously-created LoggerCallback instance object
DETAILS
Same as write4 except with 2 arguments rather than 4.
SEE
LoggerCallback_write4() // instance |
![](../../Arrow_up.png) |
Process a log event with up to 4 arguments
ARGUMENTS
handle
handle of a previously-created LoggerCallback instance object
evt
event to be logged
mid
module ID of the module which logged the event
a1
arbitrary argument passed by caller
DETAILS
The
evt argument is of type Log.Event, which encodes the
Log.EventId, the
Diags.Mask, and the
Diags.EventLevel of the event. The event ID can be obtained
via
Types.getEventId(evt), the Diags mask can be obtained via
Diags.getMask(evt), and the event level can be obtained via
Diags.getLevel(evt).
The modId argument is the module ID of the module that logged the
event.
The event information can be used by the logger to handle different
events specially. For example, the event ID can be used to compare
against other known Log.Events.
if (Log_getEventId(MY_EVENT) == Log_getEventId(evt)) {
:
}
The Diags mask and event level can be used for filtering of events
based on event level (see
IFilterLogger), or even routing
events to separate loggers based on diags category (see, for example,
LoggerBuf.statusLogger).
The Diags mask and event level are useful for handling the event, but
are generally not recorded by the logger because they are not needed in
decoding and displaying the event. A more suitable value to record is a
Types.Event, which encodes the event ID and module ID. For
example, the
Log.EventRec type stores a
Types.Event
in its record definition. A
Types.Event can be created using
the
Types.makeEvent API given the event ID and module ID.
The event ID value of
0 is used to indicate an event triggered by a
call to one of the
Log_print[0-6] methods. These
methods take a format string rather than a
Log_Event argument and,
as a result, the event ID encoded in
evt is
0 and the parameter
a1 is the format string.
Non-zero event IDs can also be used to access the
msg string
associated with the
Log.EventDesc that originally
defined the
Log event.
Log_EventId id = Log_getEventId(evt));
if (id != 0) {
String msg = Text_ropeText(id);
System_aprintf(msg, a1, a2, a3, a4);
}
This works because an event's ID is simply an offset into a table
of characters (maintained by the
Text module)
containing the event's msg string.
The arguments a1, a2, etc. are parameters that are to be interpreted
according to the message format string associated with evt.
SEE
LoggerCallback_write8() // instance |
![](../../Arrow_up.png) |
Process a log event with up to 8 arguments
Void LoggerCallback_write8(
LoggerCallback_Handle handle,
Log_Event evt,
Types_ModuleId mid,
IArg a1,
IArg a2,
IArg a3,
IArg a4,
IArg a5,
IArg a6,
IArg a7,
IArg a8);
ARGUMENTS
handle
handle of a previously-created LoggerCallback instance object
DETAILS
Same as write4 except with 8 arguments rather than 4.
SEE
Instance Convertors |
![](../../Arrow_up.png) |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
![](../../Arrow_up.png) |
Int LoggerCallback_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
config LoggerCallback.createInstFxn // module-wide |
![](../../Arrow_up.png) |
User supplied logger instance create function
XDCscript usage |
meta-domain |
LoggerCallback.createInstFxn = UArg(*)(UArg) "&xdc_runtime_LoggerCallback_defaultCreate";
DETAILS
This function is called when the
LoggerCallback.create is
called.
By default, this function is configured with a default create function.
The default create function returns 0 always.
C SYNOPSIS
config LoggerCallback.outputFxn // module-wide |
![](../../Arrow_up.png) |
User supplied character callback function
XDCscript usage |
meta-domain |
LoggerCallback.
outputFxn =
Void(*)(UArg,Log.EventRec*,Int) "&xdc_runtime_LoggerCallback_defaultOutput";
DETAILS
This function is called when the
Log module needs to output an event.
e.g.
Log.write4() or
Log.print2()
By default, this function is configured with a default output function.
The default function does nothing and returns.
C SYNOPSIS
metaonly config LoggerCallback.common$ // module-wide |
![](../../Arrow_up.png) |
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly LoggerCallback.getMetaArgs() // module-wide |
![](../../Arrow_up.png) |
Returns any meta data needed to support RTA
XDCscript usage |
meta-domain |
LoggerCallback.getMetaArgs(Any inst, Any instNum) returns Any
DETAILS
This meta data should be returned in the form of a structure which
can be converted into XML. This data is added to the RTA XML file
during the application's configuration, and can be accessed later
through the xdc.rta.MetaData module.
The MetaData is returned per instance of the ILogger module. The
instance object is passed to the function as the first argument.
The second argument is the index of the instance in the list of
the ILogger's static instances.
Instance Config Parameters |
![](../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new LoggerCallback.Params;
// Instance config-params object
params.arg = UArg 0;
// User supplied argument for the user supplied create function
config LoggerCallback.arg // instance |
![](../../Arrow_up.png) |
User supplied argument for the user supplied create function
XDCscript usage |
meta-domain |
var params = new LoggerCallback.Params;
...
params.arg = UArg 0;
DETAILS
This user supplied argument will be passed back as an argument to the
createInstFxn function. It can be used by the
LoggerCallback.createInstFxn function at runtime to
differentiate between the multiple logger instances configured in the
user config script.
The user can skip configuring this argument. In such a case, the
default value 0 will be passed back as an argument to the
createInstFxn function.
C SYNOPSIS
Instance Creation |
![](../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params =
new LoggerCallback.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = LoggerCallback.create(params);
// Create an instance-object
ARGUMENTS
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)